Trossen AI Configuration

In order to use the Trossen AI Kits with LeRobot, you need to identify specifications for your setup. The specifications include the IP address, model_name, and camera serial numbers. we will pass the specifications in as arguments using --robot.ip_address, --robot.type, and --robot.cameras.

The following steps will guide you on how to configure the Trossen AI Kits with LeRobot.

The configuration File for the follower arm for the Trossen AI Kits with LeRobot can be found in lerobot_trossen/packages/lerobot_robot_trossen/src/lerobot_robot_trossen.

The configuration File for the leader arm for the Trossen AI Kits with LeRobot can be found in lerobot_trossen/packages/lerobot_teleoperation_trossen/src/lerobot_teleoperation_trossen.

@RobotConfig.register_subclass("widowxai_follower_robot")
@dataclass
class WidowXAIFollowerConfig(RobotConfig):
    # IP address of the arm
    ip_address: str

    # `max_relative_target` limits the magnitude of the relative positional target vector for
    # safety purposes. Set this to a positive scalar to have the same value for all motors, or a
    # list that is the same length as the number of motors in your follower arms.
    max_relative_target: float | None = 5.0

    # Multiplier for computing minimum time (in seconds) for the arm to reach a target position.
    # The final goal time is computed as: min_time_to_move = multiplier / fps.
    # A smaller multiplier results in faster (but potentially jerky) motion.
    # A larger multiplier results in smoother motion but with increased lag.
    # A recommended starting value is 3.0.
    min_time_to_move_multiplier: float = 3.0

    # Control loop rate in Hz
    loop_rate: int = 30

    # cameras
    cameras: dict[str, CameraConfig] = field(default_factory=dict)
    # Troubleshooting: If one of your IntelRealSense cameras freeze during
    # data recording due to bandwidth limit, you might need to plug the camera
    # on another USB hub or PCIe card.

    # Joint names for the WidowX AI follower arm
    joint_names: list[str] = field(
        default_factory=lambda: [
            "joint_0",
            "joint_1",
            "joint_2",
            "joint_3",
            "joint_4",
            "joint_5",
            "left_carriage_joint",
        ]
    )

    # "Staged" positions in rad for the arm and m for the gripper
    #
    # The robot will move to these positions when first started and before the arm is sent to the
    # sleep position.
    staged_positions: list[float] = field(
        default_factory=lambda: [0, np.pi / 3, np.pi / 6, np.pi / 5, 0, 0, 0]
    )

Setup IP Address

Note

By default, the IP address for a Trossen AI arm is set to 192.168.1.2. Make sure to change the IP addresses of your Trossen AI arms to match the ones that will be passed in the arguments.

To set up the IP address for the Trossen AI Arms, you must first ensure that the arms are connected to the same network as your computer. Refer to Arm Network Setup for correct connection instructions. Once connected, you can find or configure the IP address using the configure_cleanup demo or the set_ip_method and set_manual_ip demos.

Camera Serial Number

There are two ways to set up the camera serial numbers for the Trossen AI Kits with LeRobot: using the RealSense interface or the OpenCV interface. Based on the camera interface you choose, follow the appropriate steps below to set up the camera serial numbers.

Camera serial numbers are required to uniquely identify each camera connected to your system. You will pass the cameras as a dictionary argument using --robot.cameras.

The dictionary will look like this for two cameras:

--robot.cameras="{
    cam_main: {type: intelrealsense, serial_number_or_name: "0123456789", width: 640, height: 480, fps: 30},
    cam_wrist: {type: intelrealsense, serial_number_or_name: "0123456789", width: 640, height: 480, fps: 30}
}"

We will look at setting up the specific camera types in more detail below.

  1. Open realsense-viewer

    realsense-viewer
    

    Note

    If realsense-viewer is not already installed on your machine, follow these steps on the librealsense GitHub repository to install librealsense2-utils.

  2. Plug in a single camera and check the sidebar for its entry. If it does not show up in the side bar, click Add Source and find the Intel RealSense D405 in the drop down.

    Note

    Troubleshooting: If the camera does not show up in the sidebar after plugging it in, try a hardware reset.

  3. Click on Info for the camera, find the Serial Number, and copy it.

    Realsense Viewer

    Note

    You can also find your cameras using the command

    uv run lerobot-find-cameras realsense
    
    --- Detected Cameras ---
    Camera #0:
    Name: Intel RealSense D405
    Type: IntelRealSense
    Id: 0123456789
    Serial Number: 0123456789
    Firmware Version:
    
  4. Check the saved output in outputs/captured_images to identify which serial number corresponds to which physical camera:

    realsense__0123456789.png
    [...]
    realsense__1123456789.png
    realsense__2123456789.png
    [...]
    realsense__3123456789.png
    
  5. Put the camera serial number in the appropriate dictionary item as specified above.

  6. Repeat for the rest of the cameras.

Note

For best practices on multi-camera setups, refer to Multi-Camera configurations - D400 Series Stereo Cameras .