Trossen Arm MuJoCo

Stationary AI Pick-and-Place Demo

Sim-to-Real Transfer Demo

Overview

This repository provides MuJoCo simulation environments for Trossen AI robotic arms. It includes comprehensive robot models, inverse kinematics-based control, and tools for policy execution, data collection, and visualization.

What This Repository Offers

  • MuJoCo XML models for Trossen AI robots:

    • WidowX AI (single arm manipulator)

    • Stationary AI (dual-arm stationary platform)

    • Mobile AI (dual-arm mobile manipulator)

  • Differential inverse kinematics controller for Cartesian end-effector control

  • Pick-and-place and target following demonstration scripts

  • Motion capture and joint-controlled simulation environments

  • Data collection and visualization tools for imitation learning

Tested Environment

  • Ubuntu 22.04

  • MuJoCo 3.2.3

  • Python 3.10+

Installation

  1. Clone the repository:

    git clone https://github.com/TrossenRobotics/trossen_arm_mujoco.git ~/trossen_arm_mujoco
    
  2. It is recommended to create a virtual environment before installing dependencies. Create a Conda environment with Python 3.10 or above.

    conda create --name trossen_mujoco_env python=3.10
    conda activate trossen_mujoco_env
    
  3. Install the package and required dependencies using:

    cd ~/trossen_arm_mujoco
    pip install -e .
    
  4. To verify the installation, run:

    python3 trossen_arm_mujoco/scripts/wxai_pick_place.py
    

    If the simulation window appears with the robot performing pick-and-place, the setup was successful.

    In case of any issues, please refer to the Troubleshooting section.

Assets

All robot models are located in trossen_arm_mujoco/assets/. The assets folder contains all robot models organized by robot type, along with mesh files and scene configurations.

Directory Structure

trossen_arm_mujoco/assets/
├── meshes/          # STL files for robot components
├── wxai/
│   ├── wxai_base.xml              # WidowX AI base model
│   ├── wxai_follower.xml          # WidowX AI follower arm with camera
│   ├── scene.xml                  # Basic visualization scene
│   ├── scene_wxai_pick_place.xml  # Pick-and-place scene
│   └── scene_wxai_follow_target.xml # Target following scene
├── stationary_ai/
│   ├── stationary_ai.xml          # Dual-arm stationary platform
│   ├── stationary_ai_mocap.xml    # Mocap-enabled model with weld constraints
│   ├── scene.xml                  # Basic visualization scene
│   ├── scene_stationary_ai_pick_place.xml # Pick-and-place with handoff
│   ├── scene_joint.xml            # Joint-controlled setup
│   └── scene_mocap.xml            # Motion capture-controlled setup
└── mobile_ai/
    ├── mobile_ai.xml              # Mobile base + dual-arm
    ├── scene.xml                  # Basic visualization scene
    └── scene_mobile_ai_pick_place.xml # Mobile pick-and-place

Asset Details

WidowX AI - Single-arm manipulator:

  • Base model (wxai_base.xml): 6-DOF arm

  • Follower model (wxai_follower.xml): 6-DOF arm with camera

Stationary AI - Dual-arm stationary platform:

  • Dual WXAI arms on shared base

Mobile AI - Mobile manipulator:

  • Differential drive mobile base

  • Dual WXAI arms

Motion Capture vs Joint-Controlled Environments

Motion Capture (stationary_ai/scene_mocap.xml):

  • Uses predefined mocap bodies that move the robot arms based on scripted end effector movements

  • Useful for defining task trajectories and generating reference motions

Joint Control (stationary_ai/scene_joint.xml):

  • Uses position controllers for each joint, similar to real-world robot setup

  • Used for replaying recorded trajectories with realistic joint-level control

  • Enables clean simulation visuals without mocap bodies visible in rendered output

All models are derived from URDF descriptions in TrossenRobotics/trossen_arm_description. See individual README.md files in asset folders for detailed URDF→MJCF derivation steps.

MuJoCo IK Demo Scripts

These scripts demonstrate inverse kinematics-based control for manipulation tasks.

Pick-and-Place Demonstrations

WidowX AI - Single arm pick-and-place:

python3 trossen_arm_mujoco/scripts/wxai_pick_place.py

Stationary AI - Dual-arm pick-and-place with handoff:

python3 trossen_arm_mujoco/scripts/stationary_ai_pick_place.py

Mobile AI - Mobile base navigation + dual-arm manipulation:

python3 trossen_arm_mujoco/scripts/mobile_ai_pick_place.py

Target Following Demo

Real-time end-effector tracking using differential IK:

python3 trossen_arm_mujoco/scripts/wxai_follow_target.py

Mouse Controls:

  • Double-click to select/highlight the target cube

  • Ctrl + Left-click to rotate the view

  • Ctrl + Right-click to move the target cube

The robot will track the target cube position in real-time.

Controller API

The differential inverse kinematics controller (Controller in controller.py) provides Cartesian end-effector control for all Trossen AI robots.

Key Features

  • Damped least squares differential IK for smooth motion

  • Gripper control with open/close commands

  • Support for all robot types (WidowX AI, Stationary AI, Mobile AI)

  • Position-only or full 6D pose control

Basic Usage

from trossen_arm_mujoco.src.controller import Controller, RobotType

# Initialize controller
robot = Controller(
    model=mujoco_model,
    data=mujoco_data,
    robot_type=RobotType.WXAI,  # or RobotType.STATIONARY_AI, RobotType.MOBILE_AI
    arm_joint_names=["joint_1", "joint_2", ...],
    gripper_joint_names=["left_carriage_joint"],
    ik_scale=1.0,
    ik_damping=0.03,
)

# Command end-effector pose
error = robot.set_ee_pose(
    target_position=np.array([0.3, 0.0, 0.2]),
    target_orientation=np.array([1.0, 0.0, 0.0, 0.0]),  # [w, x, y, z]
    position_only=False,
)

# Gripper control
robot.open_gripper()
robot.close_gripper()

Controller Parameters

  • ik_scale: Scaling factor for IK velocity (default: 1.0)

  • ik_damping: Damping factor for singularity avoidance (default: 0.03)

  • position_only: When True, only controls position, orientation remains free

Modules

The trossen_arm_mujoco folder contains all Python modules necessary for running simulations, executing policies, recording episodes, and visualizing results.

Simulations

  1. ee_sim_env.py

    • Loads stationary_ai/scene_mocap.xml (motion capture-based control).

    • The arms move by following the positions commanded to the mocap bodies.

    • Used for generating scripted policies that control the robot’s arms in predefined ways.

  2. sim_env.py

    • Loads stationary_ai/scene_joint.xml (position-controlled joints).

    • Uses joint controllers instead of mocap bodies.

    • Replays joint trajectories from ee_sim_env.py, enabling clean simulation visuals without mocap bodies visible in the rendered output.

Scripted Policy Execution

  1. scripted_policy.py

    • Defines pre-scripted movements for the robot arms to perform tasks like picking up objects.

    • Uses the motion capture bodies to generate smooth movement trajectories.

    • In the current setup, a policy is designed to pick up a red block, with randomized block positions in the environment.

How the Data Collection Works

The data collection process simulates robot behavior in two stages: a mocap-driven recording phase followed by a clean replay phase for observation. This pipeline allows you to define robot movements in Cartesian space, capture the corresponding joint trajectories, and then collect realistic sensor data without contaminating it with mocap artifacts.

Motion Capture Bodies

Motion capture (mocap) bodies are dummy rigid bodies welded to the final link link_6 of each robot arm. This design enables intuitive motion definition and automatic inverse kinematics resolution:

  • Welding Behavior:

    The mocap body is rigidly attached to link_6 using a weld constraint. As the mocap body moves, the simulator ensures that the robot’s end-effector follows it.

  • Cartesian Control:

    Instead of manually commanding joint angles, you move the mocap body in 3D space x, y, z using a scripted policy. The arm’s joints are automatically adjusted to follow.

  • Joint State Recording:

    As the end-effector tracks the mocap body, the simulation records the joint configurations required at each timestep. These are saved as the action trajectory.

Replay in Joint-Controlled Environment

The recorded joint trajectories are later replayed in a second scene where:

  • The mocap bodies are removed (e.g., in stationary_ai/scene_joint.xml).

  • The arm is directly controlled using joint position commands.

  • Observations are collected without the mocap artifacts.

During replay:

  • Camera feeds from multiple viewpoints are captured.

  • Joint state feedback is logged.

  • Rewards and other metadata are recorded.

Step-by-Step Process

  1. Run record_sim_episodes.py

    1. Launch the mocap-driven simulation ee_sim_env.py.

    2. Execute a scripted Cartesian policy.

    3. Save the resulting joint position trajectory.

    4. Replay the trajectory immediately in a clean joint-controlled simulation sim_env.py to collect observations.

    • Camera feeds from 4 different viewpoints

    • Joint states (actual positions during execution)

    • Actions (input joint positions)

    • Reward values indicating success or failure

    To generate and save simulation episodes, use:

python trossen_arm_mujoco/scripts/record_sim_episodes.py \
    --task_name sim_transfer_cube \
    --data_dir sim_transfer_cube \
    --num_episodes 5 \
    --onscreen_render

Arguments:

- ``--task_name``: Name of the task to execute (default: sim_transfer_cube).
- ``--num_episodes``: Number of episodes to generate (default: 1).
- ``--data_dir``: Directory where episodes will be saved (required).
- ``--root_dir``: Root directory prefix for locating ``data_dir``. Default: ``~/.trossen/mujoco/data/``
- ``--episode_len``: Number of simulation steps per episode (default: 1000).
- ``--onscreen_render``: Enables on-screen rendering. Default: False (set to True to enable).
- ``--inject_noise``: Adds noise to actions for variability. Default: False (set to True to enable).
- ``--cam_names``: Comma-separated list of camera names for image collection (default: all available cameras).

.. note::

    * The ``--task_name`` argument is used to load the corresponding configuration from :guilabel:`constants.py`.
    * You can extend ``SIM_TASK_CONFIGS`` in :guilabel:`constants.py` to support new task configurations.
    * All parameters loaded from :guilabel:`constants.py` can be individually overridden via command-line arguments.
  1. Save the Data

    All observations and metadata are saved in .hdf5 format, with one file per episode:

    ~/.trossen/mujoco/data/sim_transfer_cube/episode_0.hdf5
    ~/.trossen/mujoco/data/sim_transfer_cube/episode_1.hdf5
    

    Check the dataset structure in the Dataset Structure section for details on the saved data.

  2. Visualizing the Data

    Use the visualize_eps.py script to convert episodes into videos:

    python trossen_arm_mujoco/scripts/visualize_eps.py \
        --data_dir sim_transfer_cube \
        --output_dir videos \
        --fps 50
    

    Arguments:

    • --data_dir: Directory containing .hdf5 files (required), relative to --root_dir if provided.

    • --root_dir: Root path prefix for locating data_dir. Default: ~/.trossen/mujoco/data/

    • --output_dir: Subdirectory inside data_dir where generated .mp4 videos will be saved. Default: videos

    • --fps: Frames per second for the generated videos. Default: 50

    Note

    If you do not specify --root_dir, videos will be saved to ~/.trossen/mujoco/data/<data_dir>/<output_dir>. You can customize the output path by changing --root_dir, --data_dir, or --output_dir as needed.

  3. Sim-to-real

    To deploy the episode on real hardware, run:

    python trossen_arm_mujoco/scripts/replay_episode_real.py \
        --data_dir sim_transfer_cube \
        --episode_idx 0 \
        --fps 10 \
        --left_ip 192.168.1.5 \
        --right_ip 192.168.1.4
    

    This script:

    • Loads the selected joint trajectory (.hdf5)

    • Sends joint commands to real arms at the specified IP addresses

    • Logs the error between commanded vs actual joint positions

    • Returns both arms to home and sleep positions after execution

    Arguments:

    • --data_dir: Directory containing .hdf5 files (required), relative to --root_dir if provided.

    • --root_dir: Root directory prefix for locating data_dir. Default: ~/.trossen/mujoco/data/

    • --episode_idx: Index of the episode to replay. Default: 0.

    • --fps: Playback frame rate (Hz). Controls the action replay speed. Default: 10.

    • --left_ip: IP address of the left Trossen arm. Default: 192.168.1.5.

    • --right_ip: IP address of the right Trossen arm. Default: 192.168.1.4.

Dataset Structure

We use the HDF5 format to store the recorded data, which is efficient for large datasets and allows for easy access to specific parts of the data.

Root Attributes

  • sim A boolean attribute indicating whether the data was collected in simulation (True) or on real hardware (False).

  • observations group: Contains all the observations recorded during the simulation.

    • images subgroup: Stores image data from multiple cameras.

      • Each camera has its own dataset named after the camera (e.g., cam_name).

      • Dataset shape: (max_timesteps, 480, 640, 3), where:

        • max_timesteps: Number of timesteps in the episode.

        • 480, 640, 3: Image dimensions (height, width, RGB channels).

      • Data type: uint8 (8-bit unsigned integers for pixel values).

      • Chunked storage: (1, 480, 640, 3) for efficient access to individual timesteps.

    • qpos: Joint positions of the robot arms in radians and gripper positions in meters.

      • Shape: (max_timesteps, 16), where:

        • max_timesteps: Number of timesteps in the episode.

        • 16: Number of joints (8 per arm: 6 revolute in radians + 2 prismatic in meters).

    • qvel: Joint velocities of the robot arms in radians/s and gripper velocities in meters/s.

      • Shape: (max_timesteps, 16).

  • action: Contains the commanded joint positions (in radians) and gripper positions (in meters) for the robot arms.

    • Shape: (max_timesteps, 16), where:

      • max_timesteps: Number of timesteps in the episode.

      • 16: Number of control dimensions (8 per arm: 6 revolute joints in radians + 2 prismatic joints in meters).

Additional Data

  • Any additional data in data_dict is stored as separate datasets under the root group.

    • Each dataset is named after the corresponding key in data_dict.

    • The data is written using root[name][...] = array.

This structure ensures efficient storage and retrieval of simulation data, supporting tasks like visualization, analysis, and sim-to-real transfer.

Customization

Modifying Tasks

To create a custom task, modify ee_sim_env.py and define a new subclass of TrossenAIStationaryEETask this will be used for running the scripted policy. Implement the following methods:

  • initialize_episode(self, physics): Sets up the initial environment state, including robot and object positions.

  • get_env_state(self, physics): Defines the data to be recorded as observations from the environment.

  • get_reward(self, physics): Implements the reward function to determine task success criteria.

class CustomTask(TrossenAIStationaryEETask):
    def initialize_episode(self, physics):
        # Set up the initial state of the environment
        pass

    def get_env_state(self, physics):
        # Define the observations to be recorded
        pass

    def get_reward(self, physics):
        # Implement the reward function
        pass

Example:

class TransferCubeTask(TrossenAIStationaryEETask):
    def initialize_episode(self, physics):
        # Set up the initial state of the environment
        pass

    def get_env_state(self, physics):
        # Define the observations to be recorded
        pass

    def get_reward(self, physics):
        # Implement the reward function
        pass
def initialize_episode(self, physics: Physics) -> None:
    """
    Set up the simulation environment at the start of an episode.

    :param physics: The simulation physics engine.
    """
    self.initialize_robots(physics)
    # randomize box position
    cube_pose = sample_box_pose()
    box_start_idx = physics.model.name2id("red_box_joint", "joint")
    np.copyto(physics.data.qpos[box_start_idx : box_start_idx + 7], cube_pose)

    super().initialize_episode(physics)

Here, sample_box_pose() is a function that generates a random pose for the red box. Then we get the joint index of the red box and set its position using np.copyto(). The initialize_robots() method is called to set the initial positions of the robot arms. The super().initialize_episode(physics) call ensures that the base class’s initialization logic is executed, setting up the environment correctly.

@staticmethod
def get_env_state(physics: Physics) -> np.ndarray:
    """
    Retrieve the environment state specific to this task.

    :param physics: The simulation physics engine.
    :return: The state of the environment.
    """
    env_state = physics.data.qpos.copy()[16:]
    return env_state

The get_env_state() method retrieves the environment state, which includes the joint positions of the red box. The physics.data.qpos.copy()[16:] line extracts the joint positions starting from index 16, which corresponds to the red box’s joint positions. physics.data.qpos is a numpy array that contains the positions of all joints in the simulation. Each arm has 6 revolute joints and 2 prismatic joints for gripper. Therefore the first 16 indices are occupied by the 2 robot arms. The rest are the joint states of the red box which is a free joint.

def get_reward(self, physics: Physics) -> int:
    """
    Compute the reward based on the cube's interaction with the robot and the environment.

    :param physics: The simulation physics engine.
    :return: The computed reward.
    """
    # return whether left gripper is holding the box
    all_contact_pairs = []
    for i_contact in range(physics.data.ncon):
        id_geom_1 = physics.data.contact[i_contact].geom1
        id_geom_2 = physics.data.contact[i_contact].geom2
        name_geom_1 = physics.model.id2name(id_geom_1, "geom")
        name_geom_2 = physics.model.id2name(id_geom_2, "geom")
        contact_pair = (name_geom_1, name_geom_2)
        all_contact_pairs.append(contact_pair)
    touch_left_gripper = (
        "red_box",
        "left/gripper_follower_left",
    ) in all_contact_pairs
    touch_right_gripper = (
        "red_box",
        "right/gripper_follower_left",
    ) in all_contact_pairs
    touch_table = ("red_box", "table") in all_contact_pairs

    reward = 0
    if touch_right_gripper:
        reward = 1
    if touch_right_gripper and not touch_table:  # lifted
        reward = 2
    if touch_left_gripper:  # attempted transfer
        reward = 3
    if touch_left_gripper and not touch_table:  # successful transfer
        reward = 4
    return reward

The get_reward() method computes the reward based on the interactions between the robot arms and the red box. It checks for contact pairs between the red box and the left and right grippers, as well as the table. The reward is assigned based on the following conditions: - If the right gripper touches the red box, the reward is 1. - If the right gripper touches the red box and it is not touching the table, the reward is 2 (indicating that the box is lifted). - If the left gripper touches the red box, the reward is 3 (indicating an attempted transfer). - If the left gripper touches the red box and it is not touching the table, the reward is 4 (indicating a successful transfer).

Similarly we will also have to modify the sim_env.py file to add the new task this will be used for running the joint controlled simulation. Similar to the ee_sim_env.py file, we will have to implement the following methods:

  • initialize_episode(self, physics): Sets up the initial environment state, including robot and object positions.

  • get_env_state(self, physics): Defines the data to be recorded as observations from the environment.

  • get_reward(self, physics): Implements the reward function to determine task success criteria.

class CustomTask(TrossenAIStationaryTask):
    def initialize_episode(self, physics):
        # Set up the initial state of the environment
        pass

    def get_env_state(self, physics):
        # Define the observations to be recorded
        pass

    def get_reward(self, physics):
        # Implement the reward function
        pass

Example:

class TransferCubeTask(TrossenAIStationaryTask):
    def initialize_episode(self, physics):
        # Set up the initial state of the environment
        pass

    def get_env_state(self, physics):
        # Define the observations to be recorded
        pass

    def get_reward(self, physics):
        # Implement the reward function
        pass
def initialize_episode(self, physics: Physics) -> None:
    """
    Initializes the episode, resetting the robot's pose and cube position.

    :param physics: The MuJoCo physics simulation instance.
    """
    # TODO Notice: this function does not randomize the env configuration. Instead, set
    # BOX_POSE from outside reset qpos, control and box position
    with physics.reset_context():
        physics.named.data.qpos[:16] = START_ARM_POSE
        assert BOX_POSE[0] is not None
        physics.named.data.qpos[-7:] = BOX_POSE[0]

    super().initialize_episode(physics)

The initialize_episode() method sets the initial state of the environment, including the robot arms and the red box. The physics.named.data.qpos[:16] = START_ARM_POSE line sets the initial joint positions of the robot arms, while physics.named.data.qpos[-7:] = BOX_POSE[0] sets the position of the red box. We store the randomized box position in the BOX_POSE variable, which is passed to the initialize_episode() method. So that we can correctly set the position of the red box in the sim_env.py file whihc is used for running the joint controlled simulation.

@staticmethod
def get_env_state(physics: Physics) -> np.ndarray:
    """
    Retrieves the environment state, including joint positions and box position.

    :param physics: The MuJoCo physics simulation instance.
    :return: The environment state as a numpy array.
    """
    env_state = physics.data.qpos.copy()[16:]
    return env_state

The get_env_state() method remain the same as in the ee_sim_env.py file, retrieving the joint positions of the red box. You can change this to your liking if you want to add more information to the environment state.

def get_reward(self, physics: Physics) -> int:
    """
    Computes the reward based on whether the cube has been transferred successfully.

    :param physics: The MuJoCo physics simulation instance.
    :return: The computed reward which is whether left gripper is holding the box
    """
    all_contact_pairs = []
    for i_contact in range(physics.data.ncon):
        id_geom_1 = physics.data.contact[i_contact].geom1
        id_geom_2 = physics.data.contact[i_contact].geom2
        name_geom_1 = physics.model.id2name(id_geom_1, "geom")
        name_geom_2 = physics.model.id2name(id_geom_2, "geom")
        contact_pair = (name_geom_1, name_geom_2)
        all_contact_pairs.append(contact_pair)

    touch_left_gripper = (
        "red_box",
        "left/gripper_follower_left",
    ) in all_contact_pairs
    touch_right_gripper = (
        "red_box",
        "right/gripper_follower_left",
    ) in all_contact_pairs
    touch_table = ("red_box", "table") in all_contact_pairs

    reward = 0
    if touch_right_gripper:
        reward = 1
    # lifted
    if touch_right_gripper and not touch_table:
        reward = 2
    # attempted transfer
    if touch_left_gripper:
        reward = 3
    # successful transfer
    if touch_left_gripper and not touch_table:
        reward = 4
    return reward

The get_reward() method also remains the same as in the ee_sim_env.py file, computing the reward based on the interactions between the robot arms and the red box. You can change this to your liking if you want to add more information to the environment state.

We see that get_env_state() and get_reward() methods are the same in both files, but we have to implement them in both files because they are used in different contexts. This is because the ee_sim_env.py file is used for running the scripted policy, while the sim_env.py file is used for running the joint controlled simulation. This allows us to have different implementations of the same methods in different contexts, which is useful for customizing the behavior of the robot arms in different scenarios.

The initialize_episode() method is different in both as we randomize the box position in the ee_sim_env.py file, while in the sim_env.py file we set the box position to the value used in the ee_sim_env.py file.

Changing Policy Behavior

To define new behavior for the robotic arms, modify scripted_policy.py. Update the trajectory generation logic in PickAndTransferPolicy.generate_trajectory() or create a new class of your own.

Each movement step in the trajectory is defined by:

  • t: The time step at which the movement occurs.

  • xyz: The target position of the end effector in 3D space.

  • quat: The target orientation of the end effector, represented as a quaternion.

  • gripper: The target gripper finger position (0 to 0.044, where 0 is closed and 0.044 is fully open).

Example:

def generate_trajectory(self, ts_first: TimeStep):
    self.left_trajectory = [
        {"t": 0, "xyz": [0, 0, 0.4], "quat": [1, 0, 0, 0], "gripper": 0},
        {"t": 100, "xyz": [0.1, 0, 0.3], "quat": [1, 0, 0, 0], "gripper": 0.044}
    ]

We define some fixed and dynamic waypoints as follows:

init_mocap_pose_right = ts_first.observation["mocap_pose_right"]
init_mocap_pose_left = ts_first.observation["mocap_pose_left"]

box_info = np.array(ts_first.observation["env_state"])
box_xyz = box_info[:3]
print(f"Generate trajectory for {box_xyz=}")

gripper_pick_quat = Quaternion(init_mocap_pose_right[3:])
gripper_pick_quat = gripper_pick_quat * Quaternion(
    axis=[0.0, 1.0, 0.0], degrees=-45
)

meet_left_quat = Quaternion(axis=[1.0, 0.0, 0.0], degrees=90)

meet_xyz = np.array([0.0, 0.0, 0.3])

Here we define the initial pose of the right and left grippers using the ts_first.observation["mocap_pose_right"] and ts_first.observation["mocap_pose_left"] values. We also define the box position using the ts_first.observation["env_state"] value, which contains the joint positions of the red box. We then define the quaternion for the gripper pick pose and the meet pose using the Quaternion class from the trossen_arm_mujoco.utils module.

Adding New Environment Setups

The simulation uses XML files stored in the assets/ directory. To introduce a new environment setup:

  1. Create a new XML configuration file in assets/ with the desired object placements and constraints.

  2. Modify sim_env.py to load the new environment by specifying the new XML file.

  3. Update the scripted policies in scripted_policy.py to accommodate new task goals and constraints.

Troubleshooting

If you encounter Mesa Loader or mujoco.FatalError: gladLoadGL error issues, use the following command:

export LD_PRELOAD=/usr/lib/x86_64-linux-gnu/libstdc++.so.6