Trossen VR Teleoperation

Overview

The trossen_vr package is a C++ and Python SDK for controlling Trossen robot arms using Meta Quest VR controllers over network communication.

This package provides a complete solution for VR-based robot teleoperation, including:

  • C++ library with network communication and VR data handling

  • Python bindings for easy integration with Python workflows

  • Meta Quest VR headset application for wireless control

  • Event-driven and manual polling control patterns

  • Dual-arm support with independent deadman switches

  • Real-time pose and gripper control

Requirements

  • nlohmann/json >= 3.2

  • libtrossen_arm (for demos)

  • Python >= 3.11 (for Python bindings)

  • uv (for Python environment management)

  • CMake >= 3.15

  • C++17 compiler

Installation

System Dependencies

sudo apt install -y cmake build-essential nlohmann-json3-dev
curl -LsSf https://astral.sh/uv/install.sh | sh

Follow the libtrossen_arm C++ installation guide to install the robot driver if you want to run the demos.

Clone Repository

git clone https://github.com/TrossenRobotics/trossen_vr.git
cd trossen_vr

Build C++ Library

# Configure and build
cmake -B build
cmake --build build -j$(nproc)

# Install library and headers (optional, for use in other projects)
sudo cmake --install build

Build C++ Demos (Optional)

# Configure with demos enabled (requires libtrossen_arm)
cmake -B build -DBUILD_DEMOS=ON
cmake --build build -j$(nproc)

Build Python Bindings (Optional)

Install the Python development headers required by CMake’s Python detection:

sudo apt install -y python3-dev
# Create Python environment
uv sync

# Configure with Python bindings enabled
source .venv/bin/activate
cmake -B build -DBUILD_PYTHON=ON

# Build and install Python module
cmake --build build -j$(nproc)
sudo cmake --install build

VR Headset App

Installing the APK

The Trossen VR Teleop app can be sideloaded onto a Meta Quest headset. First, enable Developer Mode on the headset (Settings > System > Developer), then use one of the methods below.

Using Meta Quest Developer Hub (Windows only)

  1. Download and install Meta Quest Developer Hub

  2. Connect the headset to your PC via USB

  3. In MQDH, go to Device Manager > Apps > Install APK and select assets/VR_Teleop.apk

Using ADB (Linux / Ubuntu)

  1. Install ADB:

    sudo apt install adb
    
  2. Fix permissions (required on first use):

    # Create udev rules for Meta Quest
    echo 'SUBSYSTEM=="usb", ATTR{idVendor}=="2833", MODE="0666", GROUP="plugdev"' | sudo tee /etc/udev/rules.d/51-android.rules
    sudo chmod a+r /etc/udev/rules.d/51-android.rules
    
    # Reload udev rules
    sudo udevadm control --reload-rules
    sudo udevadm trigger
    
    # Restart ADB if running and reconnect headset
    adb kill-server
    adb start-server
    

    Disconnect and reconnect the headset USB cable after running these commands.

  3. Connect the headset to your PC via USB. Put the headset on. A prompt will appear inside asking you to Allow USB Debugging. Select Always allow from this computer and confirm.

  4. Verify the headset is detected:

    adb devices
    

    You should see a device listed with status device. If it shows unauthorized, re-check the Allow USB Debugging prompt inside the headset.

  5. Install the APK:

    adb install assets/VR_Teleop.apk
    

    A Success message confirms the installation completed.

Note

The app will appear in the headset’s App Library. If it is not visible, switch the library filter to Unknown Sources.

App UI

../_images/VR_Teleop_ui.jpg

VR Teleop App UI

UI Elements

Element

Description

Robot PC IP Address field

IP address of the PC running this trossen_vr library

Connect

Connect to the robot PC and start streaming arm data

Disconnect

Stop streaming (robot arm holds its last position)

Status

Live connection state: Disconnected → Connecting → Connected / Degraded

Frequency

Data receive rate in Hz (shown once connected)

Passthrough

Toggle camera passthrough view

Quit

Exit the application

Controller Shortcuts

  • Left Menu Button: Show or hide the UI panel

  • Right Meta Button: Snap the UI panel to in front of your current view

  • Grip / Hand Trigger (deadman switch): Hold to enable tracking and engage the arm. Release to pause.

Configuring the IP Address

Enter the IP address of the PC running the trossen_vr application or demo in the Robot PC IP Address field, then press Connect. The headset and PC must be on the same network.

Note

If the headset can’t connect, allow the receiver UDP port through the PC’s firewall (default: 9000/udp; update this if you changed ReceiverConfig.port):

sudo ufw allow 9000/udp

Ways of Operating

Once connected, there are two ways to use the app:

Passthrough Mode

Press the Passthrough button in the UI to enable the headset’s cameras so you can see the real world around you. The UI panel will disappear when passthrough is active. Press the Left Menu Button on the left controller to bring it back.

Direct View (Headset Removed)

Remove the headset and place it somewhere with a clear view of the controllers (overhead is recommended). This lets you observe the robot directly without a screen.

Warning

Proximity sensor limitation: Meta does not currently provide a built-in option to disable the proximity sensor from within the app, so the headset will go to sleep immediately when removed. We will update the app once Meta adds support for this. In the meantime, two workarounds are available:

  • Meta Quest Developer Hub (Windows only, up to 8 hours): Connect the headset to your PC via USB, open Meta Quest Developer Hub, and disable the proximity sensor under Device Manager > Device actions. This keeps the display on for up to 8 hours.

  • White tape method: Cover the proximity sensor (located inside the headset near the nose bridge) with a small piece of white tape to trick the sensor into thinking the headset is worn.

Demos

Important

Before running any demo, start the Trossen VR Teleop app on your Meta Quest headset, enter the IP address of the PC, and press Connect Button. The headset and PC must be on the same network.

Tip

Update the robot IP addresses in the demo source files to match your setup. The defaults are 192.168.1.4 (right arm) and 192.168.1.5 (left arm).

Controls

  • Hand/Grip Trigger: Hold to enable tracking and engage arm (deadman switch). Release to pause.

  • Index Trigger: Control gripper open/close.

  • B Button (right controller): Exit program.

Tracking and engagement happen automatically when you hold the hand trigger. Release the trigger to pause control while keeping the program running.

C++ Demos

Located in demos/cpp/:

  • event_driven_teleop: Event-driven dual-arm teleop using callback handlers. Demonstrates the Teleop API with automatic engage/pause via deadman switch.

  • manual_polling_teleop: Manual frame polling with inline state tracking. Same functionality, different implementation pattern showing direct frame access.

./build/event_driven_teleop
./build/manual_polling_teleop

Python Demos

Located in demos/python/:

uv run demos/python/event_driven_teleop.py
uv run demos/python/manual_polling_teleop.py