Software Setup

This section prepares the host PC, the computer that runs your control software and communicates with the Arm Controller.

What You Need

To get started, please make sure you have gone through the Hardware Setup.

PC Network Setup

The Trossen Arm Controller communicates with the Linux PC via Ethernet. As a result, the following network configurations are required on the Linux PC.

  • IPv4 Method: Manual

  • IP Address: Any unused IP addresses under the same subnet as the Arm Controller, e.g., 192.168.1.1

  • Subnet Mask: The same subnet mask used by the Arm Controller, e.g., 255.255.255.0

  • Other settings (Gateway, DNS, etc.) can be left as default

Note

Per factory settings, the Arm Controller uses

  • IPv4 method: Manual

  • IP address: 192.168.1.2

  • Subnet mask 255.255.255.0

  • Gateway: 192.168.1.1

  • DNS: 8.8.8.8

Installing the Drivers

A Trossen Arm can be controlled using either the C++ or Python driver.

Supported Platforms

Below is a list of compatible platforms for both the C++ and Python driver:

Ubuntu 20.04

Ubuntu 22.04

Ubuntu 24.04

MacOS 14

MacOS 15

x86_64

✅

✅

✅

arm64/aarch64

✅

✅

✅

✅

✅

Build System and Dependencies

The Trossen Arm Linux C++ driver is distributed from a build on Ubuntu 20.04 that links to glibc 2.31. It is provided as a static library and is statically linked to the following libraries:

Dependency

Version

Eigen3

3.4.0

spdlog

1.15.3

yaml-cpp

0.8.0

tinyxml2

9.0.0

console_bridge

1.0.1

urdfdom_headers

1.0.5

urdfdom

4.0.0

pinocchio

3.4.0

Boost

1.71.0

Python wheels are built for Python 3.10 ~ Python 3.13 on the supported platforms.

Python

To install and use the Python driver, follow these steps.

  1. Set up a virtual environment (optional)

    Some of the popular package and environment management tools are listed below. Please setup one that suits your needs.

  2. Install the driver

    pip install trossen-arm
    

    If you are using uv, add it to your project instead:

    uv add trossen-arm
    
  3. Run a script

    python3 my_script.py
    

C++

To install and use the C++ driver, follow these steps.

  1. Clone the repository

    git clone https://github.com/TrossenRobotics/trossen_arm.git
    
  2. Install the driver

    cd trossen_arm
    mkdir build
    cd build
    cmake .. [-DCMAKE_INSTALL_PREFIX=/path/to/install]
    make install
    

    If the CMAKE_INSTALL_PREFIX argument is specified, the driver will be installed locally.

    • static library and cmake configurations: /path/to/install/lib

    • header files: /path/to/install/include.

    Otherwise, the driver will be installed in the default locations.

    • static library and cmake configurations: /usr/local/lib

    • header files: /usr/local/include.

  3. Build a script

    Here is the file structure of a minimal CMake project.

    my_project/
    ├── CMakeLists.txt
    └── my_script.cpp
    

    The CMakeLists.txt file should have the following content.

    cmake_minimum_required(VERSION 3.10)
    
    # Set the project name and version
    project(my_project VERSION 1.0)
    
    # Specify the C++ standard
    set(CMAKE_CXX_STANDARD 17)
    set(CMAKE_CXX_STANDARD_REQUIRED True)
    
    # Find the libtrossen_arm package
    find_package(libtrossen_arm REQUIRED)
    
    # Add the executable for the test
    add_executable(my_script my_script.cpp)
    
    # Link the libtrossen_arm library to the executable
    target_link_libraries(my_script PRIVATE libtrossen_arm)
    
    # Install the executable
    install(TARGETS my_script DESTINATION bin)
    

    Build the project.

    cd my_project
    mkdir build
    cd build
    cmake .. -DCMAKE_INSTALL_PREFIX=/path/to/install
    make install
    

    Run the executable.

    ./path/to/install/bin/my_script
    

Arm Network Setup

As stated above, the Arm Controller uses the following factory network settings:

  • IPv4 method: Manual

  • IP address: 192.168.1.2

  • Subnet mask 255.255.255.0

  • Gateway: 192.168.1.1

  • DNS: 8.8.8.8

You may want to change the Arm Controller’s IP address to fit your application, for example to support multiple arms or to assign a static IP on your local network. To change the IP address, follow the set_manual_ip demo.

Tip

If you have a kit and are using a Trossen-supported framework like LeRobot, the expected IP addresses are:

Leader Left

192.168.1.3

Leader Right

192.168.1.2

Follower Left

192.168.1.5

Follower Right

192.168.1.4

Video Overview

What’s Next

After setting up the software, let’s configure the arm for your specific application. If your driver and Arm Controller firmware versions do not match, see Firmware Upgrade first.