Configuration

This section walks you through the configurations that can be set on a Trossen Arm. Properly configuring the arm for your application is crucial to ensure the arm operates as expected.

What You Need

To get started, please make sure you have gone through the Software Setup.

Overview

The configurations fall into four categories. Which category a configuration belongs to depends on two factors:

  • when the change takes effect: immediately, or at the next boot

  • whether it resets to default at the next boot

These categories are summarized in the following table.

Immediately Applied

Applied at Next Boot

Remain Unchanged After Reboot

Reset to Default After Reboot

The driver provides methods to get and set these configurations. An example of a configuration script is given here.

// Include the header files
#include "libtrossen_arm/trossen_arm.hpp"

int main(int argc, char** argv)
{
  // Create a driver object
  trossen_arm::TrossenArmDriver driver;

  // Configure the driver
  // This configuration is mandatory, including
  // - model of the arm
  // - end effector properties
  // - IP address of the arm
  // - whether to clear the existing error state if any
  // - Timeout for connection to the arm controller's TCP server in seconds
  driver.configure(...);

  // Get/set some configurations if needed
  // Here xxx can be
  // - factory_reset_flag
  // - ip_method
  // - manual_ip
  // - dns
  // - gateway
  // - subnet
  // - joint_characteristics
  // - effort_corrections
  // - friction_transition_velocities
  // - friction_constant_terms
  // - friction_coulomb_coefs
  // - friction_viscous_coefs
  // - end_effector
  // - joint_modes
  // - joint_limits
  // - motor_parameters
  // - links
  // - joints
  // - algorithm_parameter
  auto xxx = driver.get_xxx(...);
  driver.set_xxx(...);
}

Tip

We provide methods to exchange persistent configurations via a YAML file. Check out the configuration_in_yaml demo for more details.

Default Values

The default values are given in default_configurations_wxai_v0.yaml.

Note

The default value of the Joint Characteristics is calibrated at manufacturing and different for each arm.

Configuration Parameters

Here is a breakdown of how the configurations affect the behavior of the arm.

factory_reset_flag

If the factory_reset_flag is set to true, all configurations are reset to their factory default values at the next boot.

Choices: bool

Tip

See the set_factory_reset_flag demo for an example.

Ethernet Configuration

At startup, the Arm Controller tries to connect to the network. The procedure is as follows.

        flowchart LR
    A(Power on) --> B{ip_method?}
    B -->|dhcp| C(Acquire IP from DHCP server)
    B -->|manual| D(Set up ethernet according to the configurations)
    C --> E{success?}
    E -->|yes| F(Set up ethernet as DHCP server directs)
    E -->|no| D
    

ip_method

The IP method specifies whether the Arm Controller acquires its IP address from a DHCP server or uses a static IP address.

Choices: trossen_arm::IPMethod

Note

If the IP method is set to trossen_arm::IPMethod::dhcp, we expect a DHCP server to be present in the network. It can be a router or a computer with a DHCP server running.

manual_ip, dns, gateway, subnet

If the IP method is set to trossen_arm::IPMethod::manual, the manual IP address, DNS, gateway, and subnet are used.

Ranges: valid IPv4 addresses as strings

Tip

See the set_ip_method and set_manual_ip demos for configuring the network.

Joint Characteristics

The joint characteristics affect the behavior of each joint.

Tip

See the set_joint_characteristics and joint_characteristics_finetune demos for setting and tuning these.

effort_corrections

The trossen_arm::JointCharacteristic::effort_correction maps a motor’s effort unit to the standard unit, i.e., Nm and N.

To give an example, in external effort mode, the command sent to the motor is given by the following expression.

\[\text{effort}_\text{motor} = \text{effort_correction} \times \left( \text{external_effort}_\text{desired} + \text{effort}_\text{compensation} \right)\]

Vice versa, the effort returned by the driver is given by the following expression.

\[\text{external_effort} = \frac{\text{effort}_\text{motor}}{\text{effort_correction}} - \text{effort}_\text{compensation}\]

Range: \([0.2, 5.0]\)

friction_transition_velocities, friction_constant_terms, friction_coulomb_coefs, and friction_viscous_coefs

We model joint friction as a function of velocity and effort of three components: Coulomb, viscous, and constant.

  • The Coulomb friction is proportional to the magnitude of the effort.

  • The viscous friction is proportional to the velocity.

  • The constant friction is independent of the velocity and effort.

To deal with the discontinuity when the direction of the velocity changes, we use a linear transition characterized by the transition velocity.

The resulting compensation effort is given below, where \(\text{effort}_\text{inverse_dynamics}\) is the effort computed by inverse dynamics.

\[\begin{split}\text{effort}_\text{friction} &= \text{constant_term} \\ &+ \text{coulomb_coef} \times \lvert \text{effort}_\text{inverse_dynamics} \rvert \\ &+ \text{viscous_coef} \times \lvert \text{velocity} \rvert \\ \text{effort}_\text{compensation} &= \text{effort}_\text{inverse_dynamics} \\ &+ \begin{cases} + \text{effort}_\text{friction} & \text{if } \text{velocity} \gt \text{transition_velocity} \\ - \text{effort}_\text{friction} & \text{if } \text{velocity} \lt -\text{transition_velocity} \\ + \text{effort}_\text{friction} \times \frac{\text{velocity}}{\text{transition_velocity}} & \text{otherwise} \end{cases}\end{split}\]

Each controller-arm pair comes with calibrated effort corrections and friction parameters as defaults. They should work decently for most applications. However, you can always fine-tune them according to personal preferences.

Here is a guideline to tune the effort corrections and friction parameters.

  1. Put the arm in gravity compensation, i.e., all external efforts are zero

  2. Tune the joints one by one from gripper to base

Ranges:

position_offset

The trossen_arm::JointCharacteristic::position_offset offsets the joint position to account for homing error. It is added to the command sent to the motor and subtracted from the feedback received from the motor.

\(\text{position}_\text{motor} = \text{position} + \text{position_offset}\)

where \(\text{position}_\text{motor}\) is used by the motor and \(\text{position}\) is intended to match the kinematic model definition.

All transactions of positions in the driver API refer to \(\text{position}\), e.g., trossen_arm::RobotOutput::Cartesian::positions, trossen_arm::RobotOutput::Joint::All::positions, trossen_arm::TrossenArmDriver::set_cartesian_positions(), and trossen_arm::TrossenArmDriver::set_all_positions().

Range: \(\mathbb{R}\)

Warning

Since these configurations are arm specific, mixed usage of Arm Controller and arm with different serial numbers may cause deterioration in performance.

End Effector

The trossen_arm::EndEffector class lets you use different end effectors. It’s important to match the end effector properties with the actual end effector attached to the arm. Otherwise, the Arm Controller won’t be able to properly compensate for the end effector’s weight and inertia.

Tip

End effector variants supported by Trossen Robotics are provided in trossen_arm::StandardEndEffector.

Tip

New in version 1.8.3: the original rack-and-pinion end effector can be removed or replaced with a custom end effector.

On startup, the Arm Controller checks if the gripper motor exists. If the motor is not detected, it assumes that the gripper assembly has been removed. An example with nothing mounted at the flange is given by trossen_arm::StandardEndEffector::no_gripper.

What works:

  • Inverse dynamics for the arm joints, e.g., gravity and friction compensations

  • Input and output of the arm joints, e.g., Cartesian and joint positions, velocities, and efforts

What won’t work:

  • Input and output of the end effector

Finger Offsets

The offsets of the left and right fingers define the home position specific to the fingers.

For a custom end effector, these offsets are ignored.

Ranges: \(\mathbb{R}\)

pitch_circle_radius

The pitch circle radius defines the transmission ratio of the rack and pinion mechanism of the original end effector.

trossen_arm::EndEffector::pitch_circle_radius specifies pitch circle radius of the pinion of the end effector.

For a custom end effector, this value is ignored.

Range: \(\mathbb{R}\)

t_flange_tool

trossen_arm::EndEffector::t_flange_tool defines the tool frame pose measured in the flange frame as shown in the image below.

../_images/t_flange_tool.jpeg

Note

The first 3 elements are the translation and the last 3 elements are the angle-axis representation of the rotation

Range: \(\mathbb{R}^6\)

Joint Modes

The joint modes define the mode of operation of each joint.

Choices: trossen_arm::Mode

Tip

See the set_mode demo for setting joint modes.

Joint Limits

The joint limits define the operating limits of each joint.

The block diagram of the control loop of the motor is given below.

        flowchart TD
    A[ ] -->|desired position| B[clip]
    style A fill:transparent, stroke:transparent
    B -->|clipped desired position| C((sum))
    C -->|position error| D[PID]
    D -->|desired velocity| E((sum))
    E --> F[clip]
    F -->|clipped desired velocity| G((sum))
    G -->|velocity error| H[PID]
    H -->|desired effort| I((sum))
    I --> J[clip]
    J -->|clipped desired effort| K((motor))

    L[ ] -->|feedforward velocity| E
    style L fill:transparent, stroke:transparent
    M[ ] -->|feedforward effort| I
    style M fill:transparent, stroke:transparent

    K -->|actual position| N{check}
    N -->|within limit| C
    K -->|actual velocity| O{check}
    O -->|within limit| G

    N -->|beyond limit| P[error]
    O -->|beyond limit| P
    

When the Arm Controller receives a command from the driver, it generates the command for a motor by clipping to the min and max limits.

When the Arm Controller receives a feedback from the motor, it triggers an error if anything is beyond the max and min limits padded by the tolerances.

For reference, we can choose the limits as follows.

  1. When creating a new application script, we need

    • the min and max limits to be above the expected motion range

    • the tolerances to be 0.0 to catch any unexpected behavior

  2. When the application script is well tested, we need

    • the min and max limits to be above the expected motion range

    • the tolerances to be some positive values to avoid false positives

Range: \(\mathbb{R}\)

Tip

See the set_joint_limits demo for an example.

Motor Parameters

The motor parameters define the control parameters of each motor.

As shown in the block diagram above, each motor trossen_arm::MotorParameter has two PID controllers for position and velocity regulation. By setting different parameters in trossen_arm::PIDParameter, we can achieve the behavior of different trossen_arm::Mode.

Tip

Commonly used motor parameters are provided in trossen_arm::StandardMotorParameters. Check out the set_motor_parameters demo for details.

A guideline to tune the motor parameters is given below.

Ranges: \(\mathbb{R}\)

Joints

New in version 1.11.0.

The joints define the kinematic properties of every arm joint and both finger joints, in that order. Together with the Links, they define the kinematic chain used for forward and inverse kinematics as well as inverse dynamics.

Each trossen_arm::Joint places the joint frame relative to its parent link frame via trossen_arm::Joint::origin_xyz and trossen_arm::Joint::origin_rpy, and describes the motion it allows via trossen_arm::Joint::axis, the unit twist of the joint expressed in the joint frame. The first three elements of the axis are the angular component and the last three are the linear component, e.g., a joint rotating about the frame’s z axis has an axis of \((0, 0, 1, 0, 0, 0)\).

Tip

Commonly used joints are provided in trossen_arm::StandardJoints. Check out the set_joints demo for details.

Note

The lateral placement of both finger joints comes from trossen_arm::EndEffector::offset_finger_left and trossen_arm::EndEffector::offset_finger_right, which override the second element of the corresponding trossen_arm::Joint::origin_xyz stored here. See Finger Offsets.

Warning

The joints define where the arm believes its own links are. Inaccurate values degrade Cartesian tracking and gravity compensation everywhere, so change them only with a measurement to back the change.

Ranges:

Algorithm Parameter

This configuration defines the parameters used for robotic algorithms.

  • trossen_arm::AlgorithmParameter::singularity_threshold:

    When moving in Cartesian space, an error is triggered if the arm is close to a singular configuration. The threshold is defined below.

    \[\text{singularity_threshold} \lt \frac{\min_i {|\text{pivot}_i|}}{\max_i {|\text{pivot}_i|}}\]

    where \(\text{pivot}_i\) is the \(i\)’th pivot of the QR decomposition of the Jacobian that maps joint velocities to Cartesian velocities.

    Range: \(\mathbb{R}\)

What’s Next?

Now that the arm is configured, an assorted collection of Demo Scripts is available to help you get started with controlling the arm.