Configuration
This section walks you through the configurations that can be set on a Trossen AI arm. Properly configuring the arm for your application is crucial to ensure the arm operates as expected.
What You Need
To get started, please make sure you have gone through the Software Setup.
Overview
Depending on
when the change takes effect
whether the changed configuration is reset to default at the next boot
the configurations are divided into four categories as given in the following table.
Immediately Applied |
Applied at Next Boot |
|
|---|---|---|
Remain Unchanged After Reboot |
|
|
Reset to Default After Reboot |
|
|
The driver provides methods to get and set these configurations. An example of a configuration script is given here.
// Include the header files
#include "libtrossen_arm/trossen_arm.hpp"
int main(int argc, char** argv)
{
// Create a driver object
trossen_arm::TrossenArmDriver driver;
// Configure the driver
// This configuration is mandatory, including
// - model of the arm
// - end effector properties
// - IP address of the arm
// - whether to clear the existing error state if any
driver.configure(...);
// Get/set some configurations if needed
// Here xxx can be
// - factory_reset_flag
// - ip_method
// - manual_ip
// - dns
// - gateway
// - subnet
// - joint_characteristics
// - effort_corrections
// - friction_transition_velocities
// - friction_constant_terms
// - friction_coulomb_coefs
// - friction_viscous_coefs
// - continuity_factors
// - end_effector
// - gripper_force_limit_scaling_factor
auto xxx = driver.get_xxx(...);
driver.set_xxx(...);
}
# Import the driver
import trossen_arm
if __name__ == "__main__":
# Create a driver object
driver = trossen_arm.TrossenArmDriver()
# Configure the driver
# This configuration is mandatory, including
# - model of the arm
# - end effector properties
# - IP address of the arm
# - whether to clear the existing error state if any
driver.configure(...)
# Get/set some configurations if needed
# Here xxx can be
# - factory_reset_flag
# - ip_method
# - manual_ip
# - dns
# - gateway
# - subnet
# - joint_characteristics
# - effort_corrections
# - friction_transition_velocities
# - friction_constant_terms
# - friction_coulomb_coefs
# - friction_viscous_coefs
# - continuity_factors
# - end_effector
# - gripper_force_limit_scaling_factor
xxx = driver.get_xxx(...)
driver.set_xxx(...)
Tip
We provide methods to exchange persistent configurations via a YAML file. Check out the configuration_in_yaml demo for more details.
How They Work?
Here is a breakdown of how the configurations affect the behavior of the arm.
factory_reset_flag
If the factory reset flag is set to true, all configurations are reset to their factory default values at the next boot.
Default value: false
Choices: true, false
Ethernet Configuration
At startup, the arm controller tries to connect to the network. The procedure is as follows.
flowchart LR
A(Power on) --> B{ip_method?}
B -->|dhcp| C(Acquire IP from DHCP server)
B -->|manual| D(Set up ethernet according to the configurations)
C --> E{success?}
E -->|yes| F(Set up ethernet as DHCP server directs)
E -->|no| D
ip_method
The IP method can be set to dhcp or manual.
Default value: manual
Choices: dhcp, manual
Note
If the IP method is set to dhcp, we expect a DHCP server to be present in the network.
It can be a router or a computer with a DHCP server running.
manual_ip, dns, gateway, subnet
If the IP method is set to manual, the manual IP address, DNS, gateway, and subnet are used.
Default values:
manual_ip:
192.168.1.2dns:
8.8.8.8gateway:
192.168.1.1subnet:
255.255.255.0
Ranges: valid IPv4 addresses
Joint Characteristics
The joint characteristics affect the behavior of each joint.
effort_corrections
The effort corrections map the motors’ effort unit to the standard unit, i.e., Nm and N.
To give an example, in external effort mode, the command sent to the motor is given by the following expression.
Vice versa, the effort returned by the driver is given by the following expression.
Default values are arm specific and calibrated at the factory.
Range: \([0.5, 2.0]\)
friction_transition_velocities, friction_constant_terms, friction_coulomb_coefs, and friction_viscous_coefs
We model joint friction as a function of velocity and effort of three components: Coulomb, viscous, and constant.
The Coulomb friction is proportional to the magnitude of the effort.
The viscous friction is proportional to the velocity.
The constant friction is independent of the velocity and effort.
To deal with the discontinuity when the direction of the velocity changes, we use a linear transition characterized by the transition velocity.
The resulting compensation effort is given below, where \(\text{effort}_\text{inverse_dynamics}\) is the effort computed by inverse dynamics.
Each controller-arm pair comes with calibrated effort corrections and friction parameters as defaults. They should work decently for most applications. However, you can always fine-tune them according to personal preferences.
Here is a guideline to tune the effort corrections and friction parameters.
Put the arm in gravity compensation, i.e., all external efforts are zero
Tune the joints one by one from gripper to base
Increase the
effort_correctionif the links onwards are pulled down by gravityMove the joint at low velocity and increase the
friction_coulomb_coefif the resistance is stronger when the joint is compensating for gravity than in a balanced positionMove the joint at varying velocities and increase the
friction_viscous_coefif there’s more resistance at higher velocityIncrease the
friction_constant_termto uniformly reduce the resistance up til the joint starts moving spontaneouslyIncrease the
friction_transition_velocityif quiet operation and large stiction is preferred over reduced stiction with high-frequency oscillations
Default values are arm specific and calibrated at the factory.
Ranges:
friction_transition_velocities: \(\mathbb{R}_{\gt 0}\)
others: \(\mathbb{R}\)
Warning
Since these configurations are arm specific, mixed usage of controller and arm with different serial numbers may cause deterioration in performance.
continuity_factors
The arm controller uses this factor to determine whether the commanded joint position is continuous. If not, the controller enter the 16: Robot Input Discontinuous error state.
Default value: 5.0
Range: \([1.0, 10.0]\)
Tip
If you run into the 16: Robot Input Discontinuous error state, please
check that the frequency of the control loop is at least 300 Hz if the built-in interpolator is disabled, i.e., the
goal_timeis zerootherwise, check that the
goal_timeis long enough compared to looping time so that the joint can feasibly reachgoal_positionwithingoal_timefinally, if you’re confident that there’s no implementation mistake in the script, increase the continuity factor with discretion
Note
Continuity checks can be disabled by setting a joint’s continuity factor to a negative value.
Warning
This is a potentially dangerous option as it allows users to command positions to joints that far exceed physical limits. Please use it with caution.
End Effector
The trossen_arm::EndEffectorProperties allow the usage of different end effectors.
It’s important to match the end effector properties with the actual end effector attached to the arm.
Otherwise, the controller won’t be able to properly compensate for the end effector’s weight and inertia.
Tip
The commonly used trossen_arm::StandardEndEffector are provided in the driver.
Link Properties
The trossen_arm::LinkProperties members of the end effector define the three links of an end effector.
palm: the whole end effector excluding the fingers
left finger: the finger on the left side
right finger: the finger on the right side
where the mass, inertia, origin_xyz, and origin_rpy values follow the URDF convention. And the left and right sides are defined with respect to the arm’s perspective, i.e., observing from the base to the end effector when the joints are in home positions.
Finger Offsets
The offsets of the left and right fingers are required.
offset_finger_left: the offset from the palm center to the left carriage center in m with the fingers closed
offset_finger_right: the offset from the palm center to the right carriage center in m with the fingers closed
Gripper Force Limit Scaling Factor
This scaling factor scales the force limit of the gripper. The force limit is given by the following expression where \(\text{max_force}\) is the maximum force of the gripper given in Specifications.
Default value: 0.5
Range: \([0.0, 1.0]\)
What’s Next?
Now that the arm is configured, an assorted collection of Demo Scripts is available to help you get started with controlling the arm.