Hardware Setup

This section walks you through the hardware setup for a new Trossen AI Kit.

Assembly

Standalone Arm

Download the assembly guide or watch the YouTube video for your arm model and variant from the options below:

Warning

Make sure the Arm Controller is OFF before connecting any cables to it.

Warning

If using a network switch to interface with multiple arms, make sure to only the connect the devices required by your application. Low-quality connections can cause degraded performance.

Note

As an alternative to using the Base Clamp Plate, you can instead create a custom fixture using the dimensions below:

../_images/mounting_holes.png

Mobile AI Kit

Watch the YouTube video below for assembly instructions for the Mobile AI kit:

Stationary AI Kit

Watch the YouTube video below for assembly instructions for the Stationary AI kit:

What’s Next

Now that you have completed the hardware setup, you can move on to the Software Setup section to install the necessary software.