Trossen Arm Driver API
Note
These API docs are generated based on the C++ library. The Python package is not explicitly documented due to its similarity to the C++ API.
Class Hierarchy
-
- Namespace trossen_arm
- Enum InterpolationSpace
- Enum IPMethod
- Enum LogLevel
- Enum Mode
- Enum Model
- Struct AlgorithmParameter
- Struct DiscoverResult
- Struct EndEffector
- Struct Joint
- Struct JointCharacteristic
- Struct JointLimit
- Struct Link
- Struct MotorParameter
- Struct PIDParameter
- Struct RobotOutput
- Struct RobotOutput::Cartesian
- Struct RobotOutput::Header
- Struct RobotOutput::Joint
- Struct Joint::All
- Struct Joint::Arm
- Struct Joint::Gripper
- Struct StandardEndEffector
- Struct StandardJoints
- Struct StandardLinks
- Struct StandardMotorParameters
- Class LogicError
- Class RuntimeError
- Class TrossenArmDriver
- Enum ErrorState
- Enum Notice
- Namespace trossen_arm
File Hierarchy
-
- Directory include
- Directory libtrossen_arm
- File trossen_arm.hpp
- File trossen_arm_type.hpp
- Directory libtrossen_arm
- Directory include