Software Setup
This section describes how to set up the software environment.
What You Need
To get started, please make sure you have gone through the Hardware Setup.
Ethernet Setup
The Trossen Arm Controller communicates with the Linux PC via Ethernet. As a result, the following network configurations are required on the Linux PC.
IPv4 Method: Manual
IP Address: any unused IP addresses under the same subnet as the Arm Controller, e.g.,
192.168.1.1Subnet Mask: the same subnet mask used by the Arm Controller, e.g.,
255.255.255.0Other settings can be left as default
Note
Per factory settings, the Arm Controller uses
IPv4 method: Manual
IP address:
192.168.1.2Subnet mask
255.255.255.0Gateway:
192.168.1.1DNS:
8.8.8.8
Installing the Drivers
A Trossen Arm can be controlled using either the C++ or Python driver.
Supported Platforms
Below is a list of compatible platforms for both the C++ and Python driver:
Ubuntu 22.04 |
MacOS 14 |
MacOS 15 |
|
|---|---|---|---|
x86_64 |
✅ |
||
arm64/aarch64 |
✅ |
✅ |
✅ |
Python
To install and use the Python driver, follow these steps.
Set up a virtual environment (optional)
Some of the popular package and environment management tools are listed below. Please setup one that suits your needs.
Install the driver
Depending on the nature your application, you can install the driver in a virtual environment or the system environment.
Use virtual environment if the application is in pure Python
Use system environment if the application is for ROS
pip install trossen-arm
Run a script
python3 my_script.py
C++
To install and use the C++ driver, follow these steps.
Install dependencies required to build the driver
sudo apt update sudo apt install build-essential cmake git libyaml-cpp-dev
Clone the repository
git clone https://github.com/TrossenRobotics/trossen_arm.git
Install the driver
cd trossen_arm mkdir build cd build cmake .. [-DCMAKE_INSTALL_PREFIX=/path/to/install] make install
If the
CMAKE_INSTALL_PREFIXargument is specified, the driver will be installed in locally.static library and cmake configurations:
/path/to/install/libheader files:
/path/to/install/include.
Otherwise, the driver will be installed in the default locations.
static library and cmake configurations:
/usr/local/libheader files:
/usr/local/include.
Build a script
Here is the file structure of a minimal CMake project.
my_project/ ├── CMakeLists.txt └── my_script.cpp
The CMakeLists.txt file should have the following content.
cmake_minimum_required(VERSION 3.10) # Set the project name and version project(my_project VERSION 1.0) # Specify the C++ standard set(CMAKE_CXX_STANDARD 17) set(CMAKE_CXX_STANDARD_REQUIRED True) # Find the libtrossen_arm package find_package(libtrossen_arm REQUIRED) # Add the executable for the test add_executable(my_script my_script.cpp) # Link the libtrossen_arm library to the executable target_link_libraries(my_script PRIVATE libtrossen_arm) # Install the executable install(TARGETS my_script DESTINATION bin)
Build the project.
cd my_project mkdir build cd build cmake .. -DCMAKE_INSTALL_PREFIX=/path/to/install make install
Run the executable.
./path/to/install/bin/my_script
Software Upgrade
A controller firmware is compatible with a driver if their major and minor versions match exactly. For example, the driver v1.3.x is compatible with the controller firmware v1.3.x.
Typically a controller comes with the firmware compatible with the latest driver as of the manufacturing date. As a result, when a new driver is released, the controller firmware may need to be updated.
To upgrade, follow these steps.
Install the Teensy Loader CLI if not already installed
# Install the dependencies sudo apt update sudo apt install build-essential libusb-dev # Clone the repository git clone https://github.com/PaulStoffregen/teensy_loader_cli.git # Compile the source code cd teensy_loader_cli make # Copy the executable to the system path sudo cp teensy_loader_cli /usr/local/bin # Configure the udev rules sudo wget -O /etc/udev/rules.d/00-teensy.rules https://www.pjrc.com/teensy/00-teensy.rules
Flash the firmware
Connect the controller to the Linux PC with a USB to micro-USB cable.
Download the firmware at Downloads.
Unzip and flash the firmware using the following commands.
# Unzip the firmware unzip firmware-wxai_v0.zip # Flash the firmware teensy_loader_cli --mcu=TEENSY41 -s firmware-wxai_v0.hex
Warning
Upgrading the firmware will reset all configurations to the factory settings.
If you have made any customized configurations, we assume you are already familiar with Configuration using the driver.
A typical workflow is given below.
Use the driver compatible with the current firmware to backup all customized configurations.
Update the driver to the latest version.
Flash the latest firmware.
Set the customized configurations using the latest driver.
Video Overview
What’s Next
After setting up the software, let’s configure the arm for your specific application.