Software Setup

This section describes how to set up the software environment.

What You Need

To get started, please make sure you have gone through the Hardware Setup.

PC Network Setup

The Trossen Arm Controller communicates with the Linux PC via Ethernet. As a result, the following network configurations are required on the Linux PC.

  • IPv4 Method: Manual

  • IP Address: Any unused IP addresses under the same subnet as the Arm Controller, e.g., 192.168.1.1

  • Subnet Mask: The same subnet mask used by the Arm Controller, e.g., 255.255.255.0

  • Other settings (Gateway, DNS, etc.) can be left as default

Note

Per factory settings, the Arm Controller uses

  • IPv4 method: Manual

  • IP address: 192.168.1.2

  • Subnet mask 255.255.255.0

  • Gateway: 192.168.1.1

  • DNS: 8.8.8.8

Installing the Drivers

A Trossen Arm can be controlled using either the C++ or Python driver.

Supported Platforms

Below is a list of compatible platforms for both the C++ and Python driver:

Ubuntu 20.04

Ubuntu 22.04

Ubuntu 24.04

MacOS 14

MacOS 15

x86_64

✅

✅

✅

arm64/aarch64

✅

✅

✅

✅

✅

Build System and Dependencies

The Trossen Arm Linux C++ driver is distributed from a build on Ubuntu 20.04 that links to glibc 2.31. It is provided as a static library and is statically linked to the following libraries:

Dependency

Version

Eigen3

3.4.0

spdlog

1.15.3

yaml-cpp

0.8.0

tinyxml2

9.0.0

console_bridge

1.0.1

urdfdom_headers

1.0.5

urdfdom

4.0.0

pinocchio

3.4.0

Boost

1.71.0

Python

To install and use the Python driver, follow these steps.

  1. Set up a virtual environment (optional)

    Some of the popular package and environment management tools are listed below. Please setup one that suits your needs.

  2. Install the driver

    Depending on the nature your application, you can install the driver in a virtual environment or the system environment.

    • Use virtual environment if the application is in pure Python

    • Use system environment if the application is for ROS

    pip install trossen-arm
    
  3. Run a script

    python3 my_script.py
    

C++

To install and use the C++ driver, follow these steps.

  1. Clone the repository

    git clone https://github.com/TrossenRobotics/trossen_arm.git
    
  2. Install the driver

    cd trossen_arm
    mkdir build
    cd build
    cmake .. [-DCMAKE_INSTALL_PREFIX=/path/to/install]
    make install
    

    If the CMAKE_INSTALL_PREFIX argument is specified, the driver will be installed in locally.

    • static library and cmake configurations: /path/to/install/lib

    • header files: /path/to/install/include.

    Otherwise, the driver will be installed in the default locations.

    • static library and cmake configurations: /usr/local/lib

    • header files: /usr/local/include.

  3. Build a script

    Here is the file structure of a minimal CMake project.

    my_project/
    ├── CMakeLists.txt
    └── my_script.cpp
    

    The CMakeLists.txt file should have the following content.

    cmake_minimum_required(VERSION 3.10)
    
    # Set the project name and version
    project(my_project VERSION 1.0)
    
    # Specify the C++ standard
    set(CMAKE_CXX_STANDARD 17)
    set(CMAKE_CXX_STANDARD_REQUIRED True)
    
    # Find the libtrossen_arm package
    find_package(libtrossen_arm REQUIRED)
    
    # Add the executable for the test
    add_executable(my_script my_script.cpp)
    
    # Link the libtrossen_arm library to the executable
    target_link_libraries(my_script PRIVATE libtrossen_arm)
    
    # Install the executable
    install(TARGETS my_script DESTINATION bin)
    

    Build the project.

    cd my_project
    mkdir build
    cd build
    cmake .. -DCMAKE_INSTALL_PREFIX=/path/to/install
    make install
    

    Run the executable.

    ./path/to/install/bin/my_script
    

Arm Network Setup

As stated above, the Arm Controller uses the following factory network settings:

  • IPv4 method: Manual

  • IP address: 192.168.1.2

  • Subnet mask 255.255.255.0

  • Gateway: 192.168.1.1

  • DNS: 8.8.8.8

You may want to change the Arm Controller’s IP address to fit your application, e.g., you have multiple arms or want to set the IP address to a static IP address in your local network. To change the IP address, follow the set_manual_ip demo.

Tip

If you have a kit and are using a Trossen-supported framework like LeRobot, the expected IP addresses are:

Leader Left

192.168.1.3

Leader Right

192.168.1.2

Follower Left

192.168.1.5

Follower Right

192.168.1.4

Software Upgrade

A controller firmware is compatible with a driver if their major and minor versions match exactly. For example, the driver v1.3.x is compatible with the controller firmware v1.3.x.

Typically a controller comes with the firmware compatible with the latest driver as of the manufacturing date. As a result, when a new driver is released, the controller firmware may need to be updated.

To upgrade, follow these steps.

  1. Install the Teensy Loader CLI if not already installed

    # Install the dependencies
    sudo apt update
    sudo apt install build-essential libusb-dev
    
    # Clone the repository
    git clone https://github.com/PaulStoffregen/teensy_loader_cli.git
    
    # Compile the source code
    cd teensy_loader_cli
    make
    
    # Copy the executable to the system path
    sudo cp teensy_loader_cli /usr/local/bin
    
    # Configure the udev rules
    sudo wget -O /etc/udev/rules.d/00-teensy.rules https://www.pjrc.com/teensy/00-teensy.rules
    
  2. Flash the firmware

    IMPORTANT! Use the driver compatible with the current firmware to backup all configurations as in configuration_in_yaml.

    Connect the controller to the Linux PC with a USB to micro-USB cable.

    Download the new firmware at Downloads.

    Unzip and flash the new firmware using the following commands.

    # Unzip the firmware
    unzip firmware-wxai_v0.zip
    
    # Flash the firmware
    teensy_loader_cli --mcu=TEENSY41 -s firmware-wxai_v0.hex
    

Warning

The expected behavior of Configuration through a firmware upgrade is as follows.

  • Upgrade, e.g., from v1.8.x to v1.9.x

    • Fields compatible with the new firmware will be retained.

    • Fields added in the new firmware will be set to default values.

  • Downgrade, e.g., from v1.9.x to v1.8.x

    • STRONGLY NOT RECOMMENDED

    • All fields will be reset to default values.

    • Default values of arm-specific fields calibrated at manufacturing, e.g., trossen_arm::JointCharacteristic, will be replaced by one-size-fits-all values leading to degraded performance.

Video Overview

What’s Next

After setting up the software, let’s configure the arm for your specific application.