Async Inference

For asynchronous / distributed inference, LeRobot runs the policy in a separate policy server process and the robot in a client process, communicating over gRPC. This is the recommended path for slow VLA policies (π₀, π₀.₅, SmolVLA): the client keeps the robot control loop responsive while the server runs inference, and overlapping action chunks are blended on the client (real-time chunking).

Dependencies

The server and client live in upstream LeRobot, and they need dependencies the lean base install (LeRobot Installation Guide) omits:

  • async: the grpcio transport used between the server and client.

  • pi: transformers/peft, required for the π-family policies (π₀, π₀.₅).

  • smolvla: required for SmolVLA policies.

Pick the policy extra that matches your policy family: pi for the π-family, smolvla for SmolVLA. If you cloned and synced lerobot_trossen, layer these in at run time by prefixing the command with uv run --with "lerobot[async,pi]>=0.5.1" (swap pi for smolvla when serving SmolVLA; requires Python ≥ 3.12). If you consume the packages from Use in Your Own Project and declared the async / pi / smolvla extras there, omit the --with prefix and run the modules directly.

Running the Policy Server and Robot Client

The flow uses two processes. Start the policy server first, then the robot client.

  1. Start the policy server (Terminal A).

    The policy server holds the policy on the GPU and answers inference requests:

    uv run --with "lerobot[async,pi]>=0.5.1" python -m lerobot.async_inference.policy_server \
        --host=127.0.0.1 \
        --port=8080 \
        --fps=30 \
        --inference_latency=0.033 \
        --obs_queue_timeout=2
    
  2. Start the robot client (Terminal B).

    The robot client drives the hardware and streams observations to the server. The example below is for a Trossen AI Stationary (bimanual) kit; adapt --robot.type and the camera/IP arguments for your kit:

    uv run --with "lerobot[async,pi]>=0.5.1" python -m lerobot.async_inference.robot_client \
        --server_address=127.0.0.1:8080 \
        --robot.type=bi_widowxai_follower_robot \
        --robot.left_arm_ip_address=192.168.1.5 \
        --robot.right_arm_ip_address=192.168.1.4 \
        --robot.left_arm_max_relative_target=0.5 \
        --robot.right_arm_max_relative_target=0.5 \
        --robot.id=bimanual_follower \
        --robot.cameras='{
            cam_high: {type: intelrealsense, serial_number_or_name: "0123456789", width: 640, height: 480, fps: 30},
            cam_low: {type: intelrealsense, serial_number_or_name: "0123456789", width: 640, height: 480, fps: 30},
            cam_left_wrist: {type: intelrealsense, serial_number_or_name: "0123456789", width: 640, height: 480, fps: 30},
            cam_right_wrist: {type: intelrealsense, serial_number_or_name: "0123456789", width: 640, height: 480, fps: 30}
            }' \
        --task="Grab and handover the red cube to the other arm" \
        --policy_type=pi05 \
        --pretrained_name_or_path=${HF_USER}/pi05-block-transfer-lerobot \
        --policy_device=cuda \
        --actions_per_chunk=50 \
        --chunk_size_threshold=0.5 \
        --aggregate_fn_name=weighted_average
    

Notes

  • The Trossen robots auto-register: LeRobot discovers the installed lerobot_robot_trossen plugin, so --robot.type=bi_widowxai_follower_robot resolves with no manual import.

  • The model loads on the first client connection (large VLAs take 1–2 min) before the first action is produced.

  • The --task prompt must match training (π-family policies are language-conditioned).

  • --actions_per_chunk, --chunk_size_threshold, and --aggregate_fn_name control real-time chunking: how many predicted steps to execute per chunk, when to re-query the server, and how overlapping steps are blended (weighted_average).

  • The client strictly only needs lerobot[async]; using [async,pi] on both is identical and simplest.

  • Start with conservative --robot.*_max_relative_target caps and keep an e-stop within reach; remove the caps once you trust the motion.

  • Stop the client first (Ctrl-C), then the server.