Training and Evaluating a Policy

Training a Policy

To train a policy to control your robot, use the train.py script. A few arguments are required. Here is an example command:

uv run lerobot-train \
    --dataset.repo_id=${HF_USER}/trossen_ai_solo_test \
    --policy.type=act \
    --output_dir=outputs/train/act_trossen_ai_solo_test \
    --job_name=act_trossen_ai_solo_test \
    --policy.device=cuda \
    --wandb.enable=true \
    --policy.repo_id=${HF_USER}/my_policy

Explanation of the Command

  1. We provided the dataset using --dataset.repo_id=${HF_USER}/trossen_ai_xxxxxxx_test.

  2. We specified the policy with --policy.type=act, which loads configurations from configuration_act.py. This policy will automatically adapt to the number of motor states, motor actions, and cameras recorded in your dataset.

  3. We set --policy.device=cuda to train on an NVIDIA GPU. If using Apple Silicon, you can replace it with --policy.device=mps.

  4. We enabled Weights & Biases logging using --wandb.enable=true for visualizing training plots. This is optional, but if used, ensure you’re logged in by running:

    wandb login
    

Note

Training will take several hours. Checkpoints will be saved in: outputs/train/act_trossen_ai_xxxxx_test/checkpoints.

To resume training from a checkpoint, below is an example command to resume from last checkpoint of the trossen_ai_xxxxxxx_test policy:

uv run lerobot-train \
    --config_path=outputs/train/trossen_ai_xxxxxxx_test/checkpoints/last/pretrained_model/train_config.json \
    --resume=true

Training Pipeline Configuration

The training pipeline can be configured using the following parameters:

  • --dataset: Configuration for the dataset.

  • --env: Configuration for the environment. Can be None.

  • --policy: Configuration for the pre-trained policy. Can be None.

  • --job_name: Name of the job. Can be None.

  • --device: Device to use for training (e.g., cuda, cpu, mps).

  • --steps: Number of training steps to run.

  • --batch_size: Batch size for training.

  • --eval_freq: Frequency of evaluation during training.

  • --save_checkpoint: Whether to save checkpoints during training.

  • --wandb: Configuration for Weights & Biases logging.

Note

For additional configuration options, use the command below to see all available command line arguments:

uv run lerobot-train --help

Evaluating Your Policy

You can evaluate your trained policy on your robot using the script below:

uv run lerobot-record \
    --robot.type=widowxai_follower_robot \
    --robot.ip_address=192.168.1.4 \
    --robot.id=follower \
    --robot.cameras='{
        cam_main: {type: intelrealsense, serial_number_or_name: "0123456789", width: 640, height: 480, fps: 30},
        cam_wrist: {type: intelrealsense, serial_number_or_name: "0123456789", width: 640, height: 480, fps: 30}
        }' \
    --display_data=false \
    --dataset.repo_id=${HF_USER}/eval_trossen_ai_solo_test \
    --dataset.single_task="Grab the cube" \
    --policy.path=${HF_USER}/my_policy

Note

If the arms move violently during evaluation because of the policy, you can smooth out the motion by increasing the motion duration. You can do this by setting a higher multiplier using the following command-line argument: --robot.min_time_to_move_multiplier=6.0

This value controls the time to reach each goal as min_time_to_move = multiplier / fps. Lower values result in quicker but potentially jerky movement; higher values improve smoothness but increase lag. A good starting value is 3.0.

Key Differences from Training Data Recording

  1. Policy Checkpoint:

    • The command includes --policy.path, which specifies the path to the trained policy checkpoint (e.g., outputs/train/act_trossen_ai_xxxxx_test/checkpoints/last/pretrained_model).

    • If you uploaded the model checkpoint to Hugging Face Hub, you can also specify it as: --control.policy.path=${HF_USER}/act_trossen_ai_xxxxx_test.

  2. Dataset Naming Convention:

    • The dataset name now begins with eval_ (e.g., ${HF_USER}/eval_act_trossen_ai_xxxxx_test) to indicate that this is an evaluation dataset.

  3. Image Writing Process:

    • We set --num_image_writer_processes=1 instead of the default 0.

    • On some systems, using a dedicated process for writing images (from multiple cameras) allows achieving a consistent 30 FPS during inference.

    • You can experiment with different values of --num_image_writer_processes to optimize performance.

Evaluating VLA Policies

The examples above evaluate an ACT policy, which the lean base install (LeRobot Installation Guide) runs directly. VLA policies (π₀, π₀.₅, SmolVLA) need extra dependencies (transformers/peft) that the base install omits.

If you cloned and synced lerobot_trossen, layer the extras at run time by prefixing the command with uv run --with "lerobot[pi]>=0.5.1" (use [smolvla] for SmolVLA):

uv run --with "lerobot[pi]>=0.5.1" lerobot-record \
    --robot.type=widowxai_follower_robot \
    --robot.ip_address=192.168.1.4 \
    --robot.id=follower \
    --robot.cameras='{
        cam_main: {type: intelrealsense, serial_number_or_name: "0123456789", width: 640, height: 480, fps: 30}
        }' \
    --display_data=false \
    --dataset.repo_id=${HF_USER}/eval_trossen_ai_solo_test \
    --dataset.single_task="Grab the cube" \
    --policy.path=${HF_USER}/my_pi05_policy

If you use your own project (Use in Your Own Project) and declared the pi / smolvla extras there, omit the --with "lerobot[pi]>=0.5.1" prefix and run lerobot-record directly.

Note

Synchronous evaluation with lerobot-record runs the policy in the robot control loop, which large VLAs are often too slow for. For responsive on-robot VLA evaluation, prefer the Async Inference flow, which runs the policy in a separate server process.