ROS 2 Standard Software Setup
Compatible Models
The ROS Interface packages can be used with any of the Interbotix LoCoBot kits listed below. Next
to each name is the codename used to describe it in software (specifically for the robot_model
argument in launch files) and a description. There are up to four parts in a name. The first word
locobot specifies that the robot is a type of rover. The next two letters represent model type
(ex. wx for 'WidowX'). The number afterwards (ex. 200) corresponds to the length of both
the arm's forearm and upper-arm links in millimeters. Finally, the s after some numbers
signifies if that arm has six degrees of freedom. If the robot has base in it, that means that
it has no arm.
| Model Name and Store Link | Robot Documentation | Codename |
|---|---|---|
| LoCoBot Base | LoCoBot Base Documentation | locobot_base |
| LoCoBot PX100 | LoCoBot PX100 Documentation | locobot_px100 |
| LoCoBot WX200 | LoCoBot WX200 Documentation | locobot_wx200 |
| LoCoBot WX250 6DOF | LoCoBot WX250 6DOF Documentation | locobot_wx250s |
- LoCoBot Base Robot Rover (
locobot_base): equipped with a Kobuki or Create® 3 mobile base, a RealSense D435 Depth camera on a DYNAMIXEL pan-tilt servo, and a NUC Intel Computer, this rover is ready to perform some serious navigation and mapping tasks. For even more flexibility, the RPLidar A2 laser scanner can be added as well. - LoCoBot PincherX 100 Robot Rover (
locobot_px100): with all the features of the locobot_base platform, this robot steps it up a notch by including the 4DOF PincherX-100 Interbotix Arm. Now officially a mobile-manipulator, this rover can perform manipulation tasks in addition to navigating/mapping an environment. - LoCoBot WidowX 200 Robot Rover (
locobot_wx200): similar in structure to the locobot_px100 robot, this platform substitutes the PincherX 100 arm with the 5DOF WidowX-200 Interbotix Arm. With longer range, a higher payload capacity, and an extra degree of freedom, this rover makes your manipulation tasks easier to perform. - LoCoBot WidowX 250 6DOF Robot Rover (
locobot_wx250s): similar in structure to the locobot_wx200 rover, this platform substitutes the WidowX 200 arm with the 6DOF WidowX-250 6DOF Interbotix Arm. With even longer range, a higher payload capacity, and yet another degree of freedom, this platform raises the bar on research mobile-manipulators.
Requirements
Below is a list of the hardware you will need to get started:
- Keyboard, mouse, HDMI monitor, and HDMI cable
- One of the X-Series LoCoBot Kits mentioned above
- Computer running Ubuntu Linux 20.04
Software Installation
Note
Terminology:
- "Remote" - Your own personal computer (desktop, laptop, etc.)
- "Robot" or "LoCoBot" - The NUC computer on the LoCoBot
To get all the code setup, refer to the computer platform types below (currently only one option, but this may change in the future) and run the appropriate installation script. Afterwards, continue with the Installation Checks sub-section.
AMD64 Architecture
Attention
If you purchased a NUC-based ROS LoCoBot from Trossen Robotics or their distributors, note that it will come pre-installed with all required software already on it and you should not have to run the software installation yourself.
After powering on the NUC via the steps in the previous section, a login screen should appear
with locobot as the user name. Conveniently, the password is the same as the user name so
type locobot and hit Enter. Next, update the computer by performing the following
steps.
Connect to the Internet. This is as simple as clicking the Wifi icon on the top right of the Desktop and selecting your desired network.
Press Ctrl + Alt + T to open a terminal screen, and type
sudo apt update.After the process completes, type
sudo apt -y upgrade. It might take a few minutes for the computer to upgrade.Finally, type
sudo apt -y autoremoveto get rid of unnecessary software packages. Then close out of the terminal and reboot the computer.Once rebooted, login and open up a terminal as before. Instead of manually installing all the software needed for the robot, you will download and run an installation script. Follow the commands below to get started! Note that no sensors or actuators (i.e. camera, lidar, U2D2, etc.) needs to be connected to the computer for the installation to work. Specify the version of ROS that you want to install using the
-dflag followed by the distribution's codename. Alternatively, you can run it without the-dflag and the script will install packages for the ROS 1 distribution supported by the version of Ubuntu. See the list of currently supported distributions. You will also need to specify the base type using the-bflag followed bycreate3if using the Create® 3 base, orkobukiif using the Kobuki base. The commands below demonstrate the process of running the installation script for ROS 2 Galactic and a Create® 3 base.$ sudo apt install curl $ curl 'https://raw.githubusercontent.com/Interbotix/interbotix_ros_rovers/main/interbotix_ros_xslocobots/install/amd64/xslocobot_amd64_install.sh' > xslocobot_amd64_install.sh $ chmod +x xslocobot_amd64_install.sh $ ./xslocobot_amd64_install.sh -d galactic -b create3
Note
The install script provides more in-depth control of some installation options. Append the
-hflag to see the help document like below:$ ./xslocobot_amd64_install.sh -h USAGE: ./xslocobot_amd64_install.sh [-h][-d DISTRO][-p PATH][-b BASE_TYPE][-n] ...
Once the script is done, shutdown the computer, and remove the HDMI cable, keyboard, and mouse. Replug any sensors into the computer that were unplugged initially. Then turn the computer on again by pressing the power button.
Remote Install
For some robotic projects, you may want to run your robot in a 'headless' state on some computer
(like a NUC or Raspberry Pi), and monitor the robot's state (in RViz for example) on your personal
(a.k.a remote) computer over a local network. For this to work, run the installation script below
on your personal computer running Linux Ubuntu 20.04. Specify the version of ROS that you want to
install using the -d flag followed by the distribution's codename. Alternatively, you can run
it without the -d flag and the script will install packages for the ROS 1 distribution
supported by the version of Ubuntu. See the list of currently supported distributions. You will
also need to specify the base type using the -b flag followed by create3 if using the
Create® 3 base, or kobuki if using the Kobuki base. The commands below demonstrate the process
of running the installation script for ROS 2 Galactic and a Create® 3 base.
Note
ROS 2, RViz, and rosdep must already be installed on your local machine for the remote install to be successful. We recommend installing ROS 2 using the Ubuntu (Debian) method described in the ROS docs.
$ sudo apt install curl
$ curl 'https://raw.githubusercontent.com/Interbotix/interbotix_ros_rovers/main/interbotix_ros_xslocobots/install/xslocobot_remote_install.sh' > xslocobot_remote_install.sh
$ chmod +x xslocobot_remote_install.sh
$ ./xslocobot_remote_install.sh -d galactic -b create3
Note
The install script provides more in-depth control of some installation options. Append the
-h flag to see the help document like below:
$ ./xslocobot_remote_install.sh -h
USAGE: ./xslocobot_remote_install.sh [-h][-d DISTRO][-p PATH][-b BASE_TYPE][-r HOSTNAME]
...
To SSH from your remote to the robot computer, first connect your personal Linux computer to the same network to which the locobot is connected. Then open a terminal and SSH into the locobot by typing (assuming a NUC-based locobot)...
$ ssh -X [email protected]
You will be prompted for a password - just type locobot and you should be in!
The -X flag in the command above allows window forwarding. This means that it's possible to
open small graphical applications on the locobot computer which will be forwarded to your personal
computer. Let's open the terminal application by...
$ gnome-terminal &
Note
Sometimes the command above doesn't work to open new terminals. An alternate solution is to use the command found in this StackExchange answer:
$ /usr/bin/dbus-launch /usr/bin/gnome-terminal &
Now, we can open up new terminals (via Ctrl + Alt + T) on the LoCoBot computer without having to SSH each time. Note that unless otherwise stated, all the following commands should be executed in the new terminal window that pops up.
Installation Checks
Note
These sensors should be plugged back in and turned on at this point if they're not already.
After running the installation script on the robot computer, verify that it was successful in
finding the U2D2, Kobuki (if applicable), and Lidar (if applicable) by checking that the port names
show up as ttyDXL, kobuki (if applicable), and rplidar (if applicable) respectively.
$ ls /dev | grep ttyDXL
ttyDXL
$ ls /dev | grep rplidar # if applicable
rplidar
If using the Create® 3 as a base, use the below command to ping the base to ensure that your network is properly configured to use the 192.168.186.2 to connect to the base. The base must be turned on and its Ethernet cable should be plugged into the NUC.
$ ping -c 2 192.168.186.2 # if applicable (robot uses the Create® 3 as its base)
PING 192.168.186.2 56(84) bytes of data.
64 bytes from 192.168.186.2: icmp_seq=1 ttl=64 time=0.040 ms
64 bytes from 192.168.186.2: icmp_seq=2 ttl=64 time=0.035 ms
--- localhost ping statistics ---
2 packets transmitted, 2 received, 0% packet loss, time 1012ms
rtt min/avg/max/mdev = 0.035/0.037/0.040/0.002 ms
Verify that the RealSense camera can be found by typing rs-enumerate-devices -S in the
terminal. The output should give info about the type of RealSense camera that is plugged in. Note
that the camera should be plugged back in at this point if it's not already.
Next Steps
If the ROS Interface installed properly, you can continue on to the ROS Interface Quickstart Guide.
Troubleshooting
Refer to the X-Series Troubleshooting Guide to try to solve your problem. If you still need help, feel free to open an Issue on the ros_rovers repo. We strongly recommend the latter option though so that other people who may be facing the same difficulty can benefit. This repository is actively maintained and any open Issues will be addressed as soon as possible.