interbotix_xs_driver
View Package on GitHub
Overview
The Interbotix X-Series Driver provides low-level interfaces to easily control the DYNAMIXEL servos on any Interbotix X-Series Robot.
Usage
The X-Series Driver is compiled as a library and can be used in any C++ project by simply including its headers and linking against it.
#include "interbotix_xs_driver/xs_logging.hpp" // Logging macros and utils
#include "interbotix_xs_driver/xs_common.hpp" // Common variables and types
#include "interbotix_xs_driver/xs_driver.hpp" // The InterbotixDriverXS class
find_package(interbotix_xs_driver REQUIRED)
add_executable(your_executable)
ament_target_dependencies(your_executable interbotix_xs_driver ...)
Then create an InterbotixDriverXS object, providing the following in the order stated:
- Absolute filepath to the motor configs file
- Absolute filepath to the mode configs file
- A boolean indicating whether the Driver should write to the EEPROM on startup
- A string indicating the driver’s logging level containing one of the following: “DEBUG”, “INFO”, “WARN”, “ERROR”, “FATAL”
This initialization would look something like below:
std::unique_ptr<InterbotixDriverXS> xs_driver = std::make_unique<InterbotixDriverXS>(
filepath_motor_configs,
filepath_mode_configs,
write_eeprom_on_startup,
logging_level);
See the package’s source code for more details.