Trossen AI Data Collection UI

Trossen AI Data Collection UI

Overview

The Trossen AI Data Collection UI is a Python-based graphical user interface (GUI) designed for seamless and efficient robotic data collection. It allows users to easily manage robot configurations, record tasks, and streamline data collection with real-time feedback, camera views, task management, and progress tracking. This documentation provides a comprehensive guide to setting up, installing, and using the Trossen AI Data Collection UI, including all its features and functionalities.

Pre-Installation Setup

Before installing the application, complete the following setup steps:

  1. Install Miniconda:

    Download and install Miniconda, a minimal installer for Conda. It simplifies package management and deployment of Python environments. Download Miniconda

  2. Create a Virtual Environment:

    Use Miniconda to create and activate a virtual environment to ensure a clean setup for the application:

    conda create -n trossen_ai_data_collection_ui_env python=3.10 -y
    conda activate trossen_ai_data_collection_ui_env
    
  3. Verify Python Version:

    Ensure that Python 3.10 is activated in the environment by running:

    python --version
    

    You should see Python 3.10.x as the output.

Installation

Once the pre-installation setup is complete, install the Trossen AI Data Collection UI Application.

  1. Install build dependencies on Linux:

    sudo apt-get install -y \
        build-essential \
        cmake \
        libavcodec-dev \
        libavdevice-dev \
        libavfilter-dev \
        libavformat-dev \
        libavutil-dev \
        libswresample-dev \
        libswscale-dev \
        pkg-config \
        python3-dev
    

    For other systems, see: Compiling PyAV.

  2. Install the application:

    pip install trossen_ai_data_collection_ui
    

    Note

    The command above requires sudo privileges and may prompt you for your password.

Post-Installation

After the installation process, run the post-installation script to complete the setup:

The post-installation script sets up additional configurations, including:

  1. Cloning and installing required dependencies for Interbotix/lerobot.

  2. Resolving common issues with OpenCV and video encoding libraries.

  3. Creating a desktop icon for easy access to the application.

Run the following command to complete the post-installation setup:

trossen_ai_data_collection_ui_post_install

Once the desktop icon is created, right-click on it and select Allow Launching to ensure the application has the necessary permissions to run.

Launching the Application

Once the installation and post-installation setup are complete, you can launch the Trossen AI Data Collection UI through either the desktop application or via the command line.

  1. Desktop Application

    After installation, a desktop shortcut named Trossen AI Data Collection UI will be available on your desktop. Simply click the shortcut to launch the application.

  2. Command Line

    Alternatively, you can run the application directly from the terminal:

    trossen_ai_data_collection_ui
    

Configuring the Robots

The Trossen AI Data Collection UI provides a user-friendly interface for configuring robot settings such as camera serial numbers and arm IP addresses. To configure the robot, follow these steps:

  1. Launch the application and click on Edit in the top-left menu. Then select Robot Configuration.

  2. In the Robot Configuration window, you will be able to modify the YAML file that contains all robot-specific settings.

  3. Update the relevant fields such as camera serial numbers and arm IP addresses as needed.

We support three robot configurations trossen_ai_stationary, trossen_ai_mobile, and trossen_ai_solo.

An example configuration for the stationary robot is shown below:

trossen_ai_stationary:

    max_relative_target: null

    min_time_to_move_multiplier: 3.0

    camera_interface: 'opencv'

    leader_arms:
        right:
            ip: '192.168.1.3'
            model: 'V0_LEADER'
        left:
            ip: '192.168.1.2'
            model: 'V0_LEADER'

    follower_arms:
        right:
            ip: '192.168.1.5'
            model: 'V0_FOLLOWER'
        left:
            ip: '192.168.1.4'
            model: 'V0_FOLLOWER'

    cameras:
        cam_high:
            serial_number: 000123456789
            width: 640
            height: 480
            fps: 30
        cam_low:
            serial_number: 000123456789
            width: 640
            height: 480
            fps: 30
        cam_right_wrist:
            serial_number: 000123456789
            width: 640
            height: 480
            fps: 30
        cam_left_wrist:
            serial_number: 000123456789
            width: 640
            height: 480
            fps: 30
  • max_relative_target: Limits the magnitude of the relative positional target vector for safety purposes. Set this to a positive scalar to have the same value for all motors. The magnitude defines the maximum distance (in radians for rotational joints and meters for linear joints) that the end-effector can be commanded to move in a single command. When you feel more confident with teleoperation or running the policy, you can extend this safety limit and even remove it by setting it to null.

  • min_time_to_move_multiplier: Multiplier for computing minimum time (in seconds) for the arm to reach a target position. The final goal time is computed as: min_time_to_move = multiplier / fps. A smaller multiplier results in faster (but potentially jerky) motion. A larger multiplier results in smoother motion but with increased lag. A recommended starting value is 3.0.

  • camera_interface: Set this according to the camera interface you want to use.

    • opencv is the default and recommended option.

    • intel_realsense can be used if you have Intel RealSense cameras connected to the system.

  • leader_arms: Contains the IP addresses and models of the leader arms.

    • ip: Update the IP addresses to match those assigned to your leader arms.

    • model: The currently supported leader arm model is V0_LEADER.

  • follower_arms: Contains the IP addresses and models of the follower arms.

    • ip: Update the IP addresses to match those assigned to your follower arms.

    • model: The currently supported follower arm model is V0_FOLLOWER.

    Note

    Refer to Setup IP Address for more details on obtaining IP addresses.

  • cameras: The cameras section defines the configuration for each camera used in the system. Each camera entry (such as cam_high, cam_low, cam_right_wrist, and cam_left_wrist) includes:

    • serial_number: The unique identifier for the camera device. For intel_realsense cameras, use the actual device serial number (e.g., 123456789). For opencv cameras, specify the camera index (e.g., 0, 1, 2).

    • width: The width of the camera image in pixels.

    • height: The height of the camera image in pixels.

    • fps: The desired frames per second for capturing images.

    Note

    • Do not change the camera names (e.g., cam_high, cam_low, etc.) as they are referenced in the application for creating predefined robot layouts.

    • Ensure that the specified FPS is supported by the camera hardware.

    • Larger resolutions may require more processing power and could impact the overall system performance.

Configuring the Tasks

The Trossen AI Data Collection UI allows users to configure various tasks for data collection. To configure tasks, follow these steps:

  1. Launch the application and click on Edit in the top-left menu. Then select Task Configuration.

  2. In the Task Configuration window, you will be able to modify the YAML file that contains all task-specific settings.

  3. Update the relevant fields such as task names, parameters, and other configurations as needed.

An example configuration for tasks is shown below:

- task_name: "trossen_ai_stationary_dummy"
  robot_model: "trossen_ai_stationary"
  task_description: "A dummy task for the Trossen AI Stationary robot."
  episode_length_s: 10
  warmup_time_s: 5
  reset_time_s: 5
  hf_user: "YourUser"
  fps: 30
  push_to_hub: false
  play_sounds: true
  disable_active_ui_updates: false
  save_interval: 1
  operators:
  - name: "YourOperator0"
    email: "[email protected]"
  - name: "YourOperator1"
    email: "[email protected]"
  • task_name: Name of the task. This should be unique for each task. This will also set the name of the dataset.

  • robot_model: The robot model associated with the task. This should match one of the robot configurations defined in the robot configuration YAML.

  • task_description: A brief description of the task.

  • episode_length_s: Duration of each episode in seconds.

  • warmup_time_s: Time in seconds to wait before starting the episode.

  • reset_time_s: Time in seconds to wait after the episode ends before resetting.

  • hf_user: Your Hugging Face username. This is used if you plan to push data to the Hugging Face Hub.

  • fps: Frames per second for data collection.

  • push_to_hub: Boolean flag indicating whether to push the collected data to the Hugging Face Hub.

  • play_sounds: Boolean flag indicating whether to play sounds during the task.

  • disable_active_ui_updates: Boolean flag to disable active UI updates during the task.

  • save_interval: Interval in episodes at which to encode images to video and save data to disk. For example, if set to 5, data will be saved every 5 episodes. Default is 1 (save after every episode). Setting save interval to -1, 0, or > total number of episodes will only save data at the end of the entire data collection session.

  • operators: Optional list of operators involved in the task. The operator information will be saved in info.json in the metadata folder. You can add multiple operators by specifying their names and email addresses. You can add, remove, or edit operators at any time; the most recent changes to the operator list will be reflected in the metadata.

    • name: Name of the operator.

    • email: Optional email address of the operator.

Note

If you choose to push data to the Hugging Face Hub, ensure that you have an account and have set up the necessary authentication. Check out the Logging into Hugging Face for more details on generating and using access tokens.

Note

The video encoding process can be resource-intensive. This can cause longer wait times between episodes, especially if you are recording at longer episode lengths. To mitigate this, consider adjusting the save_interval parameter to save data less frequently or at the end of the entire session.

Experimental Features

Note

The following features are experimental and may not be fully stable. Use them at your own discretion.

  1. GPU Acceleration for Video Encoding

    The application supports GPU acceleration for video encoding using NVIDIA GPUs with CUDA support. To enable this feature, ensure that you have the necessary NVIDIA drivers and CUDA toolkit installed on your system. You can enable GPU acceleration by setting the LEROBOT_GPU_ENCODING environment variable.

    export LEROBOT_GPU_ENCODING=1
    

    You can also choose the GPU device by setting the LEROBOT_GPU_ID environment variable to the desired GPU index (default is 0).

    export LEROBOT_GPU_ID=0
    

    The GOP (Group of Pictures) size for video encoding can be adjusted by setting the LEROBOT_GOP_SIZE environment variable (default is 30). A smaller GOP size can lead to better video quality but may increase file size. GPU encoding requires the GOP size to be a multiple of the FPS.

    export LEROBOT_GOP_SIZE=30
    

Application Features

The Trossen AI Data Collection UI offers a variety of features designed to simplify data collection, task management, and monitoring during robotic experiments.

  1. Task Management

    • Task Names: Select predefined tasks from a dropdown menu, making it easy to start data collection for specific robotic tasks.

    • Episodes: Specify the number of episodes for the current task using the spin box. You can increase or decrease the count using the + and - buttons.

  2. Recording Controls

    • Start Recording: Initiates the data collection for the selected task, beginning the recording of robot actions.

    • Stop Recording: Ends the current data collection session.

    • Re-Record: Enables the user to re-record the current episode in case of any errors during data collection, so bad episodes can be skipped and the dataset stays clean.

  3. Progress Tracking

    • The GUI includes a progress bar that tracks the data collection session in real-time, displaying the percentage of completion.

  4. Camera Views

    • Live Camera Feeds: You can view multiple camera angles at once while recording, making it easy to monitor the robotic arms and their surroundings as things happen.

  5. Configuration Management

    • Edit Robot Configuration: The robot’s YAML settings—like camera serial numbers and arm IP addresses—can be easily updated through the GUI, giving users detailed control over the robot’s configuration.

    • Edit Task Configuration: Task-specific parameters can be adjusted via a YAML editor to tailor the task according to experiment requirements.

  6. Quit Button

    • The application features a Quit button in the menu that lets you exit safely, making sure all your data is saved and everything shuts down properly.

Troubleshooting

Arms Jittering

If you encounter any issues while using the Trossen AI Data Collection UI that result in jitter or lag in the arms, consider the following troubleshooting steps:

Check System Resources

Ensure that your system has sufficient CPU and memory resources available. Close any unnecessary applications that may be consuming resources.

Explicitly Set Camera Interface to opencv

If you are using Intel RealSense cameras and experience lag, try changing the camera interface to opencv in the robot configuration YAML file. This can help reduce latency associated with the RealSense SDK.

Adjust min_time_to_move_multiplier

If the arms are moving too fast or jerkily, consider adjusting the min_time_to_move_multiplier in the robot configuration YAML file. A smaller value can lead to faster movements, while a larger value can result in smoother but slower motions.

Disable Active UI Updates

If you notice significant lag during data collection, try enabling the disable_active_ui_updates option in the task configuration YAML file. This can help improve performance by reducing the load on the GUI during recording.

Disable Camera Views

If the camera views are causing lag, consider disabling them temporarily to see if performance improves. This just disables the camera feeds in the GUI but does not affect data collection. Click the checkbox labeled Disable Camera Views in the top-right corner of the GUI.