Troubleshooting

This section explains the common issues while using the Trossen Arm and the corresponding solutions.

Expected Error Handling Behavior

Depending on when the error occurs, the Trossen Arm exhibits different behaviors.

Timing of Error

Expected Behavior

At startup

  • The controller LED flashes red

  • LEDs on the joints are solid red

  • Joints don’t output any torque

During operation

  • The controller LED is solid red

  • LEDs on the joints are solid green

  • The arm joints are brake-on

  • The gripper closes with a safe force

Specific Error States

The next step is to identify and resolve the specific error state.

After carrying out the proposed solution, please do one of the following.

  • restart the controller (recommended)

  • clear the error at the driver’s configure(...) call

If the problem persists, please submit a support ticket at Trossen Robotics Support.

Select the error code from the list below to view the description and solution:

0: None

Description: No error.

Solution: No action needed.

1: Ethernet Init Failed

Description: Controller’s Ethernet manager failed to initialize.

Solution: Check the network connection.

2: CAN Init Failed

Description: Controller’s CAN interface failed to initialize.

Solution: Check the controller to arm connection.

3: Joint Command Failed

Description: Controller’s CAN interface failed to send a message.

Solution: Check the controller to arm connection.

4: Joint Feedback Failed

Description: Controller’s CAN interface failed to receive a message.

Solution: Check the controller to arm connection.

5: Joint Clear Error Failed

Description: Joint clear error command failed.

Solution: Check the controller to arm connection.

6: Joint Enable Failed

Description: Joint enable command failed.

Solution: Check the controller to arm connection.

7: Joint Disable Failed

Description: Joint disable command failed.

Solution: Check the controller to arm connection.

8: Joint Set Home Failed

Description: Joint home calibration command failed.

Solution: Check the controller to arm connection.

9: Joint Disabled Unexpectedly

Description: Joint disabled unexpectedly.

Solution: Check the controller to arm connection.

10: Joint Overheated

Description: Joint overheated.

Solution: Turn off the controller to cool down the joint.

11: Invalid Mode

Description: Invalid mode command received.

Solution: Check that the driver version matches the controller firmware version.

12: Invalid Robot Command

Description: Invalid robot command indicator received.

Solution: Check that the driver version matches the controller firmware version.

13: Invalid Configuration Address

Description: Invalid configuration address.

Solution: Check that the driver version matches the controller firmware version.

14: Robot Input Mode Mismatch

Description: Robot input with modes different than configured modes received.

Solution: Verify that the sent joint inputs match the configured modes.

15: Joint Limit Exceeded

Description: Joint limit exceeded.

Solution: Check that the joint inputs are within the joint limits. Please refer to Joint Limits for how the joint limits work.

16: Robot Input Infinite

Description: Robot input with infinite values received.

Solution: Check that the joint inputs are finite. Possible causes are:

  • Incorrect scripting logic

  • The robot is close to a singular configuration while operating in Cartesian space