Home Point
DobotSCStudio supports moving the cobot to common points:
- Factory Posture: The posture in which you received the cobot. This posture reduces the cobot space, making it easy to pack and transport.
- Home Posture: The posture in which all joints are at their zero position. In this posture, the robot will be completely vertical if mounted on a horizontal surface.
- Custom Posture: A posture that is user-defined, making it easy to go back to a point that you commonly have the cobot in.
To move to any of these postures, simply hold down the button for the desired posture.