Aloha Solo Training & Evaluation
Note
ACT Solo is supported exclusively with Aloha 2.0. There is no support for Aloha Solo on Aloha 1.0. Ensure that you are using compatible software versions to avoid any issues during training or evaluation.
Install Dependencies
Install the necessary dependencies inside your containerized environment:
$ pip install dm_control==1.0.14
$ pip install einops
$ pip install h5py
$ pip install ipython
$ pip install matplotlib
$ pip install mujoco==2.3.7
$ pip install opencv-python
$ pip install packaging
$ pip install pexpect
$ pip install pyquaternion
$ pip install pyyaml
$ pip install rospkg
$ pip install torch
$ pip install torchvision
Clone ACT Solo Repository
Clone ACT Solo if using Aloha Solo
$ cd ~
$ git clone https://github.com/Interbotix/act_solo.git act_training_evaluation
Build and Install ACT Solo Models
├── act
│ ├── assets
│ ├── constants.py
│ ├── detr
│ ├── ee_sim_env.py
│ ├── imitate_episodes.py
│ ├── __init__.py
│ ├── policy.py
│ ├── record_sim_episodes.py
│ ├── scripted_policy.py
│ ├── sim_env.py
│ ├── utils.py
│ └── visualize_episodes.py
├── COLCON_IGNORE
├── conda_env.yaml
├── LICENSE
└── README.md
Navigate to the detr directory inside the repository and install the detr module which contains the model definitions using the below command:
$ cd /path/to/act_solo/ && pip install -e .
Training
To start the training, follow the steps below:
Sanity Check:
Ensure you have all the hdf5 episodes located in the correct folder after following the data collection steps Task Creation.
Source ROS Environment:
$ source /opt/ros/humble/setup.bash $ source interbotix_ws/install/setup.bash
Activate Virtual Environment:
$ source act/bin/activate
Start Training
$ cd /path/to/act/repository/ $ python3 imitate_episodes.py \ --task_name aloha_solo_dummy \ --ckpt_dir <ckpt dir> \ --policy_class ACT \ --kl_weight 10 \ --chunk_size 100 \ --hidden_dim 512 \ --batch_size 8 \ --dim_feedforward 3200 \ --num_epochs 2000 \ --lr 1e-5 \ --seed 0
Note
task_nameargument should match one of the task names in thetasks_config.yaml, as configured in the Task Creation section.ckpt_dir: The relative location where the checkpoints and best policy will be stored.policy_class: Determines the choice of policy ‘ACT’/’CNNMLP’.kl_weight: Controls the balance between exploration and exploitation.chunk_size: Determines the length of the action sequence. K=1 is no action chunking and K=episode length is full open loop control.batch_size: Low batch size leads to better generalization and high batch size results in slower convergence but faster training time.num_epochs: Too many epochs lead to overfitting; too few epochs may not allow the model to learn.lr: Higher learning rate can lead to faster convergence but may overshoot the optima, while lower learning rate might lead to slower but stable optimization.
Tip
We recommend the following parameters:
| Parameter | Value |
|---|---|
| Policy Class | ACT |
| KL Weight | 10 |
| Chunk Size | 100 |
| Batch Size | 2 |
| Num of Epochs | 3000 |
| Learning Rate | 1e-5 |
Evaluation
To evaluate a trained model, follow the steps below:
Bringup the ALOHA
Configure the environment
$ source /opt/ros/humble/setup.bash # Configure ROS system install environment $ source interbotix_ws/install/setup.bash # Configure ROS workspace environment $ source /<path_to_aloha_venv>/bin/activate # Configure ALOHA Python environment $ cd ~/<act_repository>/act_solo/
Run the evaluation script
python3 imitate_episodes.py \ --task_name aloha_solo_dummy \ --ckpt_dir <ckpt dir> \ --policy_class ACT \ --kl_weight 10 \ --chunk_size 100 \ --hidden_dim 512 \ --batch_size 8 \ --dim_feedforward 3200 \ --num_epochs 2000 \ --lr 1e-5 \ --seed 0 \ --eval \ --temporal_agg
Note
- The
task_nameargument should match one of the task names in thetasks_config.yaml, as configured in the Task Creation section. - The
ckpt_dirargument should match the correct relative directory location of the trained policy. - The
evalflag will set the script into evaluation mode. - The
temporal_aggis not required, but helps to smoothen the trajectory of the robots.