Warning
You are viewing the documentation for a version of the Interbotix ALOHA stack that is no longer supported. Please upgrade to keep up to date with the latest features. See the v2.0 documentation for more information.
Troubleshooting
Important
This guide assumes that the latest version of the software packages is used. Before proceeding, please check that they are up to date.
X-Series Arms
See the guides on the X-Series Arms documentation site.
SLATE Base
See the guides on the SLATE Base documentation site.
Device Connection Issues
USB Hubs
If using an ALOHA version with the Sabrent 7-Port USB Hubs and fail to see all connected devices when running bringup, check the following steps:
- Check that all cables are fully inserted into their ports on both ends.
- Check that all buttons corresponding to occupied ports are pressed. The LEDs should be lit and the button should be depressed.
- We have found that, occasionally, switching the port that a cable is plugged into can resolve connection issues. Make sure that the button of the now empty port is pressed again so that it is released, and that the button of the now occupied port has been depressed.