Troubleshooting
SLATE Base Error Codes
The following table lists common errors that can be indicated on the base’s screen, their cause, and their solution.
| Error Name | Code | Cause | Solution |
|---|---|---|---|
| Emergency Stop | E-Stop | Emergency stop button is pressed | Release E-Stop button |
| Communication Error | Err18 | CAN bus communication is offline | Contact support |
| Collision Error | Collision | Collision sensor triggered | Remove SLATE base from its collision |
| Battery Undervoltage | U-Vol | Battery voltage too low | Charge the SLATE base |
| Battery Overvoltage | O-Vol | Battery voltage too high | If using the original battery, overvoltage can be ignored |
| Driver Error | Err25 | Malfunctioning driver | Contact support |
| Drive Overvoltage | Err26 | Drive voltage is too high | If using the original battery, this should not occur |
| Drive Undervoltage | Err27 | Drive voltage is too low | If using the original battery, this should not occur |
| Drive Overtemperature | Err28 | High drive temperature | Contact support |
| Drive Overcurrent | Err29 | Drive motor current is too high | Contact support |
| Drive servo out of tolerance | Err30 | Drive motor is out of tolerance | Contact support |
| Drive Overload | Err31 | Drive current has exceeded 200% of rated load | Check if the wheels are blocked. Contact support |
| Encoder Error | Err32 | Drive encoder signal is malformed | Contact support |
| Hall Error | Err33 | The Hall sensor signal is malformed | Contact support |
SLATE driver can’t connect to base
dialout Group
Make sure that your user is added to the dialout group.
You can do this by running the following command:
$ sudo usermod -aG dialout $USER
Then log out and log back in for the changes to take effect.
brltty Package
The USB-Serial converter device shares the same vendor and product ID with some braille readers.
Because of this, the brltty program may claim the device, preventing its use by other drivers.
Solving this issue is as simple as removing the package using apt.
$ sudo apt-get remove brltty
Jetson Systems
The driver for the CH341 USB-Serial converter is not installed on modern Jetson systems by default. The guide below shows how to install it on Jetson systems running Jetpack 6.2 and Jetpack 6.2.1.