Data Collection
Task Creation
Task configuration can be found in the ALOHA package’s aloha module under constants.py in the TASK_CONFIGS dictionary.
A template task (aloha_template) is provided containing all possible fields and some placeholder values.
Here, we will focus only on the task name, the dataset directory, the episode length, and the observation cameras.
| Configuration Field | Description |
|---|---|
| Task Name | The task name should accurately describe the task that the ALOHA is performing. |
| Dataset Directory | The dataset_dir field sets the directory episodes will saved to. |
| Episode Length | The episode_len field sets the length of the episode in number of timesteps. |
| Camera Names | The camera_names field takes in a list of strings corresponding to camera names.
These camera names will be used as observation sources during dataset collection. |
Recording Episodes
To record an episode, follow the steps below:
- Bringup the ALOHA control stack according to your platform
- Configure the environment and run the episode recording script as follows:
$ source /opt/ros/humble/setup.bash # configure ROS system install environment $ source ~/interbotix_ws/install/setup.bash # configure ROS workspace environment $ cd ~/interbotix_ws/src/aloha/scripts/ $ python3 record_episodes.py \ --task_name <task_name> \ [--episode_idx <episode_idx>] \ [-b, --enable_base_torque] \ [-g, --gravity_compensation]The
task_nameargument should match one of the task names in theTASK_CONFIGS, as configured in the Task Creation section.The
episode_idxargument is optional and specifies the index of the episode to record reflected in the output filename<dataset_dir>/episode_<episode_idx>.hdf5. If not provided, the script will automatically calculate the next episode index based on the number of episodes already saved in the dataset directory.If the
-b, --enable_base_torqueargument is set, mobile base will be torqued on during episode recording, allowing the use of a joystick controller or some other manual method.If the
-g, --gravity_compensationargument is set, gravity compensation will be enabled for the leader robots when teleop starts.Tip
Each platform has a “dummy” task that can be used to test basic data collection and playback. For the Stationary variant, use the
aloha_stationary_dummytask. For the Mobile variant, use thealoha_mobile_dummytask.An example for the Mobile variant would look like:
$ python3 record_episodes.py --task_name aloha_mobile_dummy --episode_idx 0
Episode Playback
To play back a previously-recorded episode, follow the steps below:
- Bringup the ALOHA control stack according to your platform
- Configure the environment and run the episode playback script as follows:
$ source /opt/ros/humble/setup.bash # configure ROS system install environment $ source ~/interbotix_ws/install/setup.bash # configure ROS workspace environment $ cd ~/interbotix_ws/src/aloha/scripts/ $ python3 replay_episodes.py --dataset_dir </path/to/dataset> --episode_idx <episode_idx>Tip
An example for replaying the dummy Mobile episode recorded above would look like:
$ python3 replay_episodes.py --dataset_dir ~/aloha_data/aloha_mobile_dummy/ --episode_idx 0
Episode Auto-Recording
A helpful bash script, auto_record.sh, is provided to allow users to collect many episodes consecutively without having to interact with the control computer.
Configuration
This script, whose source can be found on the ALOHA GitHub repository, has a few configuration options that should be verified or set before running.
ROS_DISTRO
Set the codename of the ROS distribution used on the control computer.
This value is used to set the path to the ROS_SETUP_PATH variable used later in the script.
ROS_DISTRO defaults to humble.
ROS_DISTRO=humble
ROS_SETUP_PATH
Set the path to the ROS distribution’s setup script.
This value is used when setting up the system-installed ROS environment.
Setting the ROS_DISTRO variable from before should be sufficient to configure this variable.
ROS_SETUP_PATH defaults to "/opt/ros/$ROS_DISTRO/setup.bash".
ROS_SETUP_PATH="/opt/ros/$ROS_DISTRO/setup.bash"
WORKSPACE_SETUP_PATH
Set the path to the Interbotix workspace’s setup script.
This value is used when setting up the Interbotix workspace’s ROS environment.
WORKSPACE_SETUP_PATH defaults to "$HOME/interbotix_ws/install/setup.bash".
WORKSPACE_SETUP_PATH="$HOME/interbotix_ws/install/setup.bash"
RECORD_EPISODES
Set the path to the record_episodes.py script.
This value is used when calling the record_episodes script.
RECORD_EPISODES defaults to "$HOME/interbotix_ws/src/aloha/scripts/record_episodes.py".
RECORD_EPISODES="$HOME/interbotix_ws/src/aloha/scripts/record_episodes.py"
Usage
Once configured, the auto_record script is now ready to use. To auto-record a specific amount of episodes, follow the steps below:
Bringup the ALOHA control stack according to your platform
In a new terminal, navigate to the directory storing the auto_record script and run the command below:
$ auto_record.sh <task_name> <num_episodes> [-b, --enable_base_torque] [-g, --gravity_compensation]
Tip
An example for auto-recording 50 episodes of the dummy Mobile ALOHA task would look like:
$ auto_record.sh aloha_mobile_dummy 50
The auto_record script will then call the record_episodes Python script the specified number of times.
Note
If episodes of the specified task already exist, episode indices will be automatically calculated as one greater than the number of tasks in the episode save directory.
Dataset Format
ALOHA saves its episodes in the hdf5 format with the following format:
- images
- cam_high (480, 640, 3) 'uint8'
- cam_low (480, 640, 3) 'uint8' (on Stationary)
- cam_left_wrist (480, 640, 3) 'uint8'
- cam_right_wrist (480, 640, 3) 'uint8'
- qpos (14,) 'float64'
- qvel (14,) 'float64'
action (14,) 'float64'
base_action (2,) 'float64' (on Mobile)
What’s Next?
With the data collected, we are ready to train and evaluate the machine learning models.