Training and Evaluating a Policy
Training a Policy
To train a policy to control your robot, use the train.py script. A few arguments are required. Here is an example command:
python lerobot/scripts/train.py \
--dataset.repo_id=${HF_USER}/trossen_ai_stationary_test \
--policy.type=act \
--output_dir=outputs/train/act_trossen_ai_stationary_test \
--job_name=act_trossen_ai_stationary_test \
--device=cuda \
--wandb.enable=true
python lerobot/scripts/train.py \
--dataset.repo_id=${HF_USER}/trossen_ai_mobile_test \
--policy.type=act \
--output_dir=outputs/train/act_trossen_ai_mobile_test \
--job_name=act_trossen_ai_mobile_test \
--device=cuda \
--wandb.enable=true
python lerobot/scripts/train.py \
--dataset.repo_id=${HF_USER}/trossen_ai_solo_test \
--policy.type=act \
--output_dir=outputs/train/act_trossen_ai_solo_test \
--job_name=act_trossen_ai_solo_test \
--device=cuda \
--wandb.enable=true
Explanation of the Command
We provided the dataset using
--dataset.repo_id=${HF_USER}/trossen_ai_xxxxxxx_test.We specified the policy with
--policy.type=act, which loads configurations from configuration_act.py. This policy will automatically adapt to the number of motor states, motor actions, and cameras recorded in your dataset.We set
--device=cudato train on an NVIDIA GPU. If using Apple Silicon, you can replace it with--device=mps.We enabled Weights & Biases logging using
--wandb.enable=truefor visualizing training plots. This is optional, but if used, ensure you’re logged in by running:wandb login
Note
Training will take several hours. Checkpoints will be saved in: outputs/train/act_trossen_ai_xxxxx_test/checkpoints.
Training Pipeline Configuration
The training pipeline can be configured using the following parameters:
--dataset: Configuration for the dataset.--env: Configuration for the environment. Can beNone.--policy: Configuration for the pre-trained policy. Can beNone.--output_dir: Directory to save all run outputs. If another training session is run with the same value, its contents will be overwritten unlessresumeis set to true.--job_name: Name of the job. Can beNone.--resume: Set to true to resume a previous run. Ensureoutput_diris the directory of an existing run with at least one checkpoint.--device: Device to use for training (e.g.,cuda,cpu,mps).--use_amp: Determines whether to use Automatic Mixed Precision (AMP) for training and evaluation.--seed: Seed for training and evaluation environments.--num_workers: Number of workers for the dataloader.--batch_size: Batch size for training.--eval_freq: Frequency of evaluation during training.--log_freq: Frequency of logging during training.--save_checkpoint: Whether to save checkpoints during training.--save_freq: Frequency of saving checkpoints.--offline: Configuration for offline training.--online: Configuration for online training.--use_policy_training_preset: Whether to use policy training preset.--optimizer: Configuration for the optimizer. Can beNone.--scheduler: Configuration for the learning rate scheduler. Can beNone.--eval: Configuration for evaluation.--wandb: Configuration for Weights & Biases logging.
Evaluating Your Policy
You can use the record function from lerobot/scripts/control_robot.py but with a policy checkpoint as input.
Run the following command to record 10 evaluation episodes:
python lerobot/scripts/control_robot.py \
--robot.type=trossen_ai_stationary \
--control.type=record \
--control.fps=30 \
--control.single_task="Recording evaluation episode using Trossen AI Stationary." \
--control.repo_id=${HF_USER}/eval_act_trossen_ai_stationary_test \
--control.tags='["tutorial"]' \
--control.warmup_time_s=5 \
--control.episode_time_s=30 \
--control.reset_time_s=30 \
--control.num_episodes=10 \
--control.push_to_hub=true \
--control.policy.path=outputs/train/act_trossen_ai_stationary_test/checkpoints/last/pretrained_model \
--control.num_image_writer_processes=1
python lerobot/scripts/control_robot.py \
--robot.type=trossen_ai_mobile \
--control.type=record \
--control.fps=30 \
--control.single_task="Recording evaluation episode using Trossen AI Mobile." \
--control.repo_id=${HF_USER}/eval_act_trossen_ai_mobile_test \
--control.tags='["tutorial"]' \
--control.warmup_time_s=5 \
--control.episode_time_s=30 \
--control.reset_time_s=30 \
--control.num_episodes=10 \
--control.push_to_hub=true \
--control.policy.path=outputs/train/act_trossen_ai_mobile_test/checkpoints/last/pretrained_model \
--control.num_image_writer_processes=1 \
--robot.enable_motor_torque=true
python lerobot/scripts/control_robot.py \
--robot.type=trossen_ai_solo \
--control.type=record \
--control.fps=30 \
--control.single_task="Recording evaluation episode using Trossen AI Solo." \
--control.repo_id=${HF_USER}/eval_act_trossen_ai_solo_test \
--control.tags='["tutorial"]' \
--control.warmup_time_s=5 \
--control.episode_time_s=30 \
--control.reset_time_s=30 \
--control.num_episodes=10 \
--control.push_to_hub=true \
--control.policy.path=outputs/train/act_trossen_ai_solo_test/checkpoints/last/pretrained_model \
--control.num_image_writer_processes=1
Key Differences from Training Data Recording
Policy Checkpoint:
The command includes
--control.policy.path, which specifies the path to the trained policy checkpoint (e.g., outputs/train/act_trossen_ai_xxxxx_test/checkpoints/last/pretrained_model).If you uploaded the model checkpoint to Hugging Face Hub, you can also specify it as: –control.policy.path=${HF_USER}/act_trossen_ai_xxxxx_test.
Dataset Naming Convention:
The dataset name now begins with
eval_(e.g.,${HF_USER}/eval_act_trossen_ai_xxxxx_test) to indicate that this is an evaluation dataset.
Image Writing Process:
We set
--control.num_image_writer_processes=1instead of the default0.On some systems, using a dedicated process for writing images (from multiple cameras) allows achieving a consistent 30 FPS during inference.
You can experiment with different values of
--control.num_image_writer_processesto optimize performance.