Record
This page walks through a full recording session using the example demos that ship with the SDK.
What You Need
Complete Installation and Setup and verify
make buildsucceeds.Create or edit a config file as described in Configuration.
Power on the arms, connect the cameras, and confirm the controller IPs are reachable with
ping.
Run the Demo
./build/examples/trossen_solo_ai \
--config examples/trossen_solo_ai/config.json
./build/examples/trossen_stationary_ai \
--config examples/trossen_stationary_ai/config.json
./build/examples/trossen_mobile_ai \
--config examples/trossen_mobile_ai/config.json
If you omit --config, the demo loads its default config file:
Robot |
Default config path |
|---|---|
Solo |
|
Stationary |
|
Mobile |
|
These paths are resolved relative to the directory you launch the binary from (typically the repo root).
Edit the file in place to change the default, or pass --config <path> to point at a different file.
Append --dump-config to any of the commands above to print the merged configuration and exit without touching hardware.
Episode Workflow
A recording session proceeds through the following phases:
Startup. The demo parses the config, constructs the
SessionManager, and starts the teleop thread.Staging. The operator moves the leader arm(s) to the episode start pose. The follower(s) mirror the leader continuously at the configured
teleop.rate_hz.Recording. The
SessionManageropens a new.mcapfile, starts all producers, and begins logging. The process runs for at mostsession.max_durationseconds. If your config defines anobserversblock, each observer receives the same records in parallel — see Visualize for the ReRun live-viewer setup.Reset. After each episode, the demo pauses for
session.reset_durationseconds before starting the next episode.Shutdown. After
session.max_episodesepisodes the teleop thread stops and the process exits cleanly.
Episodes are written to <backend.root>/<backend.dataset_id>/episode_NNNNNN.mcap.
Episode numbers are assigned automatically and resume from the highest existing index in the directory.
Re-running the demo against the same dataset_id appends rather than overwriting.
What Gets Recorded
Each .mcap file contains synchronized data from all producers enabled in the config.
Topic names are derived from the stream_id of each producer.
Channel |
Schema |
Content |
|---|---|---|
|
|
Joint positions (rad), velocities (rad/s), efforts (Nm) |
|
|
Width, height, encoding, pixel data |
|
|
Pose (m, rad), twist (m/s, rad/s) |
What’s Next
With .mcap episodes on disk: