Configuration
Every recording session in the Trossen SDK is driven by a single JSON configuration file.
What You Need
Before editing a config, complete Installation and Setup and have the following information available:
Arm controller IP addresses.
Camera serial numbers (for Stereolabs ZED or RealSense) or
/dev/video*paths (for V4L2 USB cameras).The mobile base serial port, if applicable.
Starting From an Example
Three reference configs ship with the SDK under examples/.
Pick the one that matches your hardware.
The rest of the docs assume you are working from one of these.
1 leader + 1 follower + 2 cameras.
Config: examples/trossen_solo_ai/config.json
2 leaders + 2 followers + 4 cameras.
Config: examples/trossen_stationary_ai/config.json
2 leaders + 2 followers + 3 cameras + SLATE mobile base.
Config: examples/trossen_mobile_ai/config.json
Schema Reference
A config is a JSON object with top-level keys, used by every example:
{
"robot_name": "my_robot", // Identifier stored in dataset metadata
"hardware": { ... }, // Physical devices
"producers": [ ... ], // Data streams (one per device channel)
"teleop": { ... }, // Leader/follower pairing
"backend": { ... }, // TrossenMCAP output settings
"observers": [ ... ], // Optional live-stream consumers (e.g. ReRun viewer)
"session": { ... } // Episode durations and limits
}
Hardware
The hardware block describes the physical devices connected to the PC.
It contains arms and cameras (always required), plus an optional mobile_base.
hardware.arms is a map of arm ID to arm config.
Each entry accepts:
Field |
Type |
Description |
|---|---|---|
|
string |
IPv4 address of the arm controller |
|
string |
Arm model, currently only |
|
string |
|
hardware.cameras is an array of camera configs.
Each entry accepts:
Field |
Type |
Description |
|---|---|---|
|
string |
User-chosen label referenced by |
|
string |
Camera serial (Stereolabs ZED or RealSense) |
|
int |
Frame resolution in pixels |
|
int |
Capture frame rate |
hardware.mobile_base (optional) accepts:
Field |
Type |
Description |
|---|---|---|
|
bool |
Zero the odometry on startup |
|
bool |
Enable base motors on startup |
Producers
producers is a JSON array.
Each entry describes one data stream that the SDK will poll and record.
Add one producer per arm, one per camera, and one per mobile base.
{
"type": "trossen_arm", // Producer type (table below)
"hardware_id": "leader", // Must match a key in hardware
"stream_id": "leader", // Label used inside the MCAP file
"poll_rate_hz": 30.0,
"use_device_time": false,
"encoding": "bgr8" // Cameras only
}
Supported producer types:
|
Description |
|---|---|
|
Trossen AI Kit arm |
|
Stereolabs ZED (Jetson only; requires |
|
RealSense RGB |
|
V4L2 USB camera (any |
|
SLATE mobile base |
Tip
Set use_device_time: true for cameras so the timestamp attached to each image is the sensor capture time rather than the host-side poll time.
For arms, false is usually fine because the host-side timestamp matches the joint-state read.
Teleop
"teleop": {
"enabled": true, // Set false to disable teleop
"rate_hz": 1000.0, // Teleop command rate
"pairs": [ // One entry per leader/follower pair
{ "leader": "<arm_id>", "follower": "<arm_id>" }
]
}
leader and follower values must match keys in hardware.arms.
Backend
"backend": {
"root": "~/.trossen_sdk", // Directory where episodes are written
"dataset_id": "my_dataset", // Sub-directory for this dataset
"compression": "", // "" | "lz4" | "zstd"
"chunk_size_bytes": 4194304 // MCAP chunk size (4 MB default)
}
Episodes land at <root>/<dataset_id>/episode_NNNNNN.mcap.
Episode numbers are assigned automatically and resume from the highest existing index in the directory.
Observers
observers is an optional JSON array of live, non-durable consumers that receive records as they are produced.
Each observer runs alongside the backend and is independent of the on-disk .mcap capture — leave the key out entirely if you do not need live streaming.
The only observer that ships with the SDK today is the ReRun viewer ("type": "rerun").
For background on what ReRun is and how to launch the viewer, see Visualize.
"observers": [
{
"type": "rerun", // Observer type (table below)
"id": "live_viewer", // Logging label; defaults to type
"enabled": true, // Set false to disable this observer
"rerun_url": "rerun+http://127.0.0.1:9876/proxy", // gRPC endpoint of a running ReRun viewer
"app_id": "trossen_solo_ai", // ReRun application id
"spawn": false, // true = SDK launches the viewer itself (ignores rerun_url)
"subscriptions": [
{ "record_id": "leader", "throttle_hz": 30.0 },
{ "record_id": "follower", "throttle_hz": 30.0 },
{ "record_id": "camera_main", "throttle_hz": 15.0 }
]
}
]
Fields common to every observer:
Field |
Type |
Description |
|---|---|---|
|
string |
Observer type. Required. Only |
|
string |
Logging label for this instance. Defaults to |
|
bool |
When |
|
array |
Per-stream subscriptions. At least one entry is required and |
Each subscription entry accepts:
Field |
Type |
Description |
|---|---|---|
|
string |
Exact match against a producer’s |
|
number |
Maximum dispatch rate to this observer for this stream. Range |
|
array of strings |
Optional per-subscription field filter. Observer-specific semantics — for |
ReRun-specific fields (used only when type is "rerun"):
Field |
Type |
Description |
|---|---|---|
|
string |
gRPC URL of an already-running ReRun viewer. Defaults to |
|
string |
ReRun application id passed to the recording stream. Defaults to |
|
bool |
When |
Note
ReRun support is a build-time option.
Configure with -DTROSSEN_ENABLE_RERUN_OBSERVER=ON to compile the observer in.
With the option off (default), any "type": "rerun" entry in your config fails to load with an “unknown observer type” error.
See Visualize for the full setup walkthrough.
Session
"session": {
"max_duration": 20.0, // Seconds per episode
"max_episodes": 50, // Total episodes to record
"backend_type": "trossen_mcap", // Selects the backend implementation
"reset_duration": 5.0 // Pause between episodes (see table)
}
reset_duration behavior:
Value |
Behavior |
|---|---|
Positive number (e.g. |
Countdown for that many seconds, then start the next episode |
|
No pause; start the next episode immediately |
Omitted / |
Wait indefinitely until the operator presses right arrow |
Configuring Your Robot
The example configs work out of the box on the reference hardware. For your own robot you will typically need to change:
Arm IP addresses. One per arm. Must match the controllers on your network.
Camera serial numbers. One per camera. Must match the physical cameras plugged in.
Dataset ID. Pick a short, unique label so episodes from different runs don’t mix.
Everything else can stay at the example defaults for a first recording. See Finding Device Identifiers below for how to look up each value.
The solo config has 2 arms and 2 cameras.
Replace the placeholders in examples/trossen_solo_ai/config.json:
"hardware": {
"arms": {
"leader": { "ip_address": "<LEADER_IP>", ... },
"follower": { "ip_address": "<FOLLOWER_IP>", ... }
},
"cameras": [
{ "id": "camera_main", "serial_number": "<MAIN_SERIAL>", ... },
{ "id": "camera_wrist", "serial_number": "<WRIST_SERIAL>", ... }
]
},
"backend": {
"dataset_id": "<YOUR_DATASET>",
...
}
The stationary config has 4 arms (left/right leader + left/right follower) and 4 cameras.
Replace the placeholders in examples/trossen_stationary_ai/config.json:
"hardware": {
"arms": {
"leader_left": { "ip_address": "<LEADER_LEFT_IP>", ... },
"leader_right": { "ip_address": "<LEADER_RIGHT_IP>", ... },
"follower_left": { "ip_address": "<FOLLOWER_LEFT_IP>", ... },
"follower_right": { "ip_address": "<FOLLOWER_RIGHT_IP>", ... }
},
"cameras": [
{ "id": "camera_high", "serial_number": "<HIGH_SERIAL>", ... },
{ "id": "camera_low", "serial_number": "<LOW_SERIAL>", ... },
{ "id": "camera_left_wrist", "serial_number": "<LEFT_WRIST_SERIAL>", ... },
{ "id": "camera_right_wrist", "serial_number": "<RIGHT_WRIST_SERIAL>", ... }
]
},
"backend": {
"dataset_id": "<YOUR_DATASET>",
...
}
Verify the teleop.pairs list matches how you physically paired the leader and follower arms.
Mismatched pairs are the most common source of mirrored-motion bugs in bimanual setups.
The mobile config has the same 4 arms as stationary, 3 cameras, and a mobile_base block.
Replace the placeholders in examples/trossen_mobile_ai/config.json:
"hardware": {
"arms": {
"leader_left": { "ip_address": "<LEADER_LEFT_IP>", ... },
"leader_right": { "ip_address": "<LEADER_RIGHT_IP>", ... },
"follower_left": { "ip_address": "<FOLLOWER_LEFT_IP>", ... },
"follower_right": { "ip_address": "<FOLLOWER_RIGHT_IP>", ... }
},
"cameras": [
{ "id": "camera_high", "serial_number": "<HIGH_SERIAL>", ... },
{ "id": "camera_left_wrist", "serial_number": "<LEFT_WRIST_SERIAL>", ... },
{ "id": "camera_right_wrist", "serial_number": "<RIGHT_WRIST_SERIAL>", ... }
],
"mobile_base": {
"reset_odometry": false,
"enable_torque": false
}
},
"backend": {
"dataset_id": "<YOUR_DATASET>",
...
}
Set mobile_base.reset_odometry to true for the first run against a fresh base so odometry starts at zero.
Leave enable_torque at false while editing.
Flip it to true once the base is in a safe spot to drive.
Finding Device Identifiers
RealSense Serial Numbers
With the RealSense SDK installed, launch the official viewer:
realsense-viewer
Each connected camera appears in the left panel. Hover over a camera’s name to see its serial number, or expand the Info section in the camera’s settings to copy it. Plug in every camera, open its live stream in the viewer, and match the feed to the serial by its field of view.
CLI Overrides
Any JSON key can be overridden at runtime using dot-notation with --set KEY=VALUE.
This is the fastest way to tweak one value without editing JSON:
./build/examples/trossen_solo_ai \
--set hardware.arms.leader.ip_address=192.168.1.2 \
--set session.max_duration=30 \
--set backend.dataset_id=trial_01
./build/examples/trossen_stationary_ai \
--set hardware.arms.leader_left.ip_address=192.168.1.3 \
--set session.max_duration=30 \
--set backend.dataset_id=trial_01
./build/examples/trossen_mobile_ai \
--set hardware.mobile_base.enable_torque=true \
--set session.max_duration=30 \
--set backend.dataset_id=trial_01
Flags can be repeated.
Overrides are applied after the JSON file is loaded and before the config is validated, so you can inspect the merged result without running hardware by appending --dump-config.
What’s Next
With a working config, continue to Record to record your first dataset.