Communication Settings

IP Setting

The LAN2 network interface’s IP address, subnet mask, and gateway can be modified in this menu. The robot can communicate with external equipment through its LAN2 network interface to devices that support TCP, UDP, and Modbus protocols. The robot must be within the same network segment as that of the external equipment and there cannot be conflict in addresses. The default IP address is 192.168.5.1.

../../_images/ip_setting.jpg

WiFi Setting

You can modify the WiFi’s name and password in this menu. The robot can communicate with external equipment through WiFi. Once set, the robot must be restarted for the change to take effect. The default password is 1234567890.

../../_images/wifi_setting.jpg