Unitree Camera SDK
This guide is intended to help users get started using the Go1 EDU using the Unitree Camera SDK.
The Unitree Camera SDK allows depth and color streaming, and provides intrinsic calibration information. The library also offers pointcloud, depth image aligned to color image.
Dependencies
| Dependency | Minimum Version | Remarks |
|---|---|---|
| OpenCV | >=4 | Requires GStreamer |
| CMake | >=2.8 | |
| OpenGL | For Pointcloud GUI | |
| GLUT | For Pointcloud GUI | |
| X11 | For Pointcloud GUI |
Workspace Setup
Clone the repository.
$ git clone https://github.com/unitreerobotics/UnitreecameraSDK.git
Build the SDK.
$ cd UnitreeCameraSDK $ mkdir build $ cd build $ cmake .. $ make
Running Examples
Note
You may have to kill processes that occupy the cameras’ resources before running the examples. To do so, run the commands given in the example_putImagetrans demo.
# If you start this file, you must bash "kill.sh" to turn off automatic startup program.
# "Unitree/autostart/02camerarosnode/kill.sh" and "Unitree/autostart/04imageai/kill.sh".
# You can also use the following instructions:
ps -A | grep point | awk '{print $1}' | xargs kill -9
ps -aux|grep mqttControlNode|grep -v grep|head -n 1|awk '{print $2}'|xargs kill -9
ps -aux|grep live_human_pose|grep -v grep|head -n 1|awk '{print $2}'|xargs kill -9
Get Camera Raw Image
$ cd UnitreeCameraSDK
$ ./bin/example_getRawFrame
Get Calibration Parameters File
$ cd UnitreeCameraSDK
$ ./bin/example_getCalibParamsFile
Get Rectified Image
$ cd UnitreeCameraSDK
$ ./bin/example_getRectFrame
Get Depth Image
$ cd UnitreeCameraSDK
$ ./bin/example_getDepthFrame
Get Point Cloud
$ cd UnitreeCameraSDK
$ ./bin/example_getPointCloud
Transfer Image to Other Devices
$ cd UnitreeCameraSDK
$ ./bin/example_putImagetrans
Get Image From Other Devices
$ cd UnitreeCameraSDK
$ ./bin/example_getimagetrans