Training and Evaluation
Virtual Environment Setup
Effective containerization is important when it comes to running machine learning models as there can be conflicting dependencies. You can either use a Virtual Environment or Conda.
Virtual Environment Installation and Setup
- Install the virtual environment package:
$ sudo apt-get install python3-venv
- Create a virtual environment:
$ python3 -m venv ~/act # Creates a venv "act" in the home directory, can be created anywhere
- Activate the virtual environment:
$ source act/bin/activate
Conda Setup
- Create a virtual environment:
$ conda create -n aloha python=3.8.10
- Activate the virtual environment:
$ conda activate aloha
Install Dependencies
Install the necessary dependencies inside your containerized environment:
$ pip install dm_control==1.0.14
$ pip install einops
$ pip install h5py
$ pip install ipython
$ pip install matplotlib
$ pip install mujoco==2.3.7
$ pip install opencv-python
$ pip install packaging
$ pip install pexpect
$ pip install pyquaternion
$ pip install pyyaml
$ pip install rospkg
$ pip install torch
$ pip install torchvision
Clone Repository
Clone ACT if using Aloha Stationary
$ cd ~
$ git clone https://github.com/Interbotix/act.git act_training_evaluation
Clone ACT++ if using Aloha Mobile
$ cd ~
$ git clone https://github.com/Interbotix/act_plus_plus.git act_training_evaluation
Build and Install ACT Models
├── act
│ ├── assets
│ ├── constants.py
│ ├── detr
│ ├── ee_sim_env.py
│ ├── imitate_episodes.py
│ ├── __init__.py
│ ├── policy.py
│ ├── record_sim_episodes.py
│ ├── scripted_policy.py
│ ├── sim_env.py
│ ├── utils.py
│ └── visualize_episodes.py
├── COLCON_IGNORE
├── conda_env.yaml
├── LICENSE
└── README.md
Navigate to the detr
directory inside the repository and install the detr module whihc contains the model definitions using the below command:
$ cd /path/to/act/detr && pip install -e .
Training
To start the training, follow the steps below:
Sanity Check:
Ensure you have all the hdf5 episodes located in the correct folder after following the data collection steps Task Creation.
Source ROS Environment:
$ source /opt/ros/humble/setup.bash $ source interbotix_ws/install/setup.bash
Activate Virtual Environment:
$ source act/bin/activate
Start Training
$ cd /path/to/act/repository/ $ python3 imitate_episodes.py \ --task_name aloha_stationary_dummy \ --ckpt_dir <ckpt dir> \ --policy_class ACT \ --kl_weight 10 \ --chunk_size 100 \ --hidden_dim 512 \ --batch_size 8 \ --dim_feedforward 3200 \ --num_epochs 2000 \ --lr 1e-5 \ --seed 0
Note
task_name
argument should match one of the task names in theTASK_CONFIGS
, as configured in the Task Creation section.ckpt_dir
: The relative location where the checkpoints and best policy will be stored.policy_class
: Determines the choice of policy ‘ACT’/’CNNMLP’.kl_weight
: Controls the balance between exploration and exploitation.chunk_size
: Determines the length of the action sequence. K=1 is no action chunking and K=episode length is full open loop control.batch_size
: Low batch size leads to better generalization and high batch size results in slower convergence but faster training time.num_epochs
: Too many epochs lead to overfitting; too few epochs may not allow the model to learn.lr
: Higher learning rate can lead to faster convergence but may overshoot the optima, while lower learning rate might lead to slower but stable optimization.
Tip
We recommend the following parameters:
Parameter | Value |
---|---|
Policy Class | ACT |
KL Weight | 10 |
Chunk Size | 100 |
Batch Size | 2 |
Num of Epochs | 3000 |
Learning Rate | 1e-5 |
Evaluation
To evaluate a trained model, follow the steps below:
Bring up the ALOHA
- Stationary: Running ALOHA Bringup
- Mobile: Running ALOHA Bringup
Configure the environment
$ source /opt/ros/humble/setup.bash # Configure ROS system install environment $ source interbotix_ws/install/setup.bash # Configure ROS workspace environment $ source /<path_to_aloha_venv>/bin/activate # Configure ALOHA Python environment $ cd ~/<act_repository>/act/
Run the evaluation script
python3 imitate_episodes.py \ --task_name aloha_stationary_dummy \ --ckpt_dir <ckpt dir> \ --policy_class ACT \ --kl_weight 10 \ --chunk_size 100 \ --hidden_dim 512 \ --batch_size 8 \ --dim_feedforward 3200 \ --num_epochs 2000 \ --lr 1e-5 \ --seed 0 \ --eval \ --temporal_agg
Note
- The
task_name
argument should match one of the task names in theTASK_CONFIGS
, as configured in the Task Creation section. - The
ckpt_dir
argument should match the correct relative directory location of the trained policy. - The
eval
flag will set the script into evaluation mode. - The
temporal_agg
is not required, but helps to smoothen the trajectory of the robots.